STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can not send data thoughout UART4 when use DCMI

Posted on January 10, 2016 at 10:56I use stm32f4 discovery connect with camera OV767 to capture picture and send it to uart4. But when i use DCMI_Cmd(ENABLE); First, i just want send 'A' but i can't. What happening with DCMI or when i use DCMI, i mu...

AdaPilot - Open Source Ada-ARM based autopilot project

Posted on January 10, 2016 at 15:11Hello STM32 Community,I would like to share with you the exiting announcement of the imminent start of the open source project AdaPilot, a safety critical autopilot for unmanned systems (drones) based on the Ada-SP...

jarno23 by Associate
  • 1033 Views
  • 0 replies
  • 0 kudos

STM32F446 SPDIFRX to I2S out possible?

Posted on December 23, 2015 at 17:38Do anybody know if STM32F446 SPDIFRX in to I2S out is possible?The worry is that input samplerate drifts and I2S output samplerate can't be changed without audible artifacts.I know that the clock PLL N and M has f...

torgeirs by Associate II
  • 2980 Views
  • 6 replies
  • 0 kudos

Keil uvision create .lib file with parameters

Posted on January 10, 2016 at 01:12Hello to all readers,i'm really out of my mind here.I searched but nothing positive.What is my purpose here. I wanna make a .lib file (hidden code to user) but still allow to set some defines in compiler preprocess...

tm3341 by Associate II
  • 1687 Views
  • 2 replies
  • 0 kudos

STM32 as bus-powered USB device: how to negotiate more power?

Posted on January 08, 2016 at 14:29According to http://www.beyondlogic.org/usbnutshell/usb2.shtml#PowerVbus, a vbus powered USB device (slave) can only pull more than 100 mA after it negotiated with the host (e.g. PC): ''High power bus powered funct...

caco3 by Associate II
  • 2779 Views
  • 3 replies
  • 0 kudos

STM32F207 EXTI Operation and Clock Confusion

Posted on January 04, 2016 at 15:59Hi,I was hoping that I might get some clarification regarding the EXTI on the STM32F207. Looking at Fig 4 (STM32F20x block diagram) within the datasheet, it would appear to be APB2; this seems to be further confirm...

STM32F745 Synchronization with GPIO

Posted on January 09, 2016 at 14:05Hey world! I use STM32F745 in my project. High-speed ADC connected to GPIO port. ADC and MCU clock from 25 MHz generator. Also clock signal goes to GPIO port. The MCU clock frequency is 200 MHz. I've realized the t...

shides2 by Associate II
  • 1645 Views
  • 3 replies
  • 0 kudos

netmf for STM32 F407

Posted on January 09, 2016 at 15:20Is there an netmf, that can be used for STM32 F4 Discovery Kit with STM32F407 MCU like .NET Micro Framework on the STM32F429 Discovery kit ? Can NET Micro Framework environment for STM32F4 microcontrollers for M...

rs.jahn9 by Associate
  • 1027 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.