2016-02-14 10:11 AM
I am trying to use HAL_SPI_TransmitReceive() to read & write to a 25AA320A SPI EEPROM.
The data was either read and/or written corrupted. The data retrieved after a write was there, but the order was scrambled (not just byte swapped). I spent days trying to understand the problem -- in both hardware and software. After digging in to the code and some online examples, I noticed that HAL_SPI_TransmitReceive() tries to read/write 16-bit values when more than one byte needs to be read or written, even with SPI_DATASIZE_8BIT.The way the code is written seems to be broken. Removing the 16-bit reads and writes when ''hspi->RxXferCount > 1'' or ''hspi->TxXferCount > 1'' allows me to read and write the EEPROM properly.Is this a known problem with this firmware version? Or is there something I am missing about how this function is used or the way the SPI peripheral needs to be configured? #stm32f3-spi-hal2016-02-17 8:08 AM
Hi riggs.rob,
The same topic is discussed [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/%5bBug%5d%20STM32F091%20HAL_SPI_TransmitReceive¤tviews=7]here. Your inputs will be helpful to conclude about the faced issue in case of 8-bits mode.As said in the other discussion, the implementation is aligned with the specification.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.