STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4xx using mic at low systicks

Posted on February 21, 2016 at 13:47Hi,I'm using the stm32f4-discovery board for recording signals utilizing the microphone.I'm configuring the clocks according to ST configuration tool ''STM32F4XX Rev A system clock configuration v1.0.1''.when conf...

haukeye by Associate II
  • 2072 Views
  • 1 replies
  • 0 kudos

How to set eclipse for STM32

Posted on February 21, 2016 at 09:06Hi,I have install toolchain and openOCD for eclipse. I have configure also.But it is showing related to PATH.here is error [code]13:27:47 **** Incremental Build of configuration Default for project encoder **** al...

stm32f4 discovery LIS3DSH HAL problem

Posted on February 16, 2016 at 14:14No answer from the register who I am. The most interesting is that this code worked for a while, but now does not work.I have attached a file that previously all worked. /* USER CODE BEGIN 0 */ uint8_t SPI_read(ui...

printf() on Nucleo-L476 board

Posted on February 19, 2016 at 19:25Hi there,I have a Nucleo-L476 board I would like to have printf() working. I used the tiny-printf provided by the Atollic IDE but I still need to implement the _write() function.Any suggestion on how this can be a...

USART gets overrun error non-stop

Posted on February 19, 2016 at 02:17I'm using STM32L4 with CubeMx.  I want to use USART3 to implement an RS232 console echo.My CubeMX is configured like this photo (and I have ''USART3 global interrupt'' checkboxed as enabled. After auto-generating ...

0690X00000604WGQAY.png
ernie by Associate
  • 1087 Views
  • 1 replies
  • 0 kudos

CAN Filters config for STM32F105 problems

Posted on February 19, 2016 at 12:32HI, I try to config Filters for two can bus on STM32F105, but i have strange problems .When i config filter with CAN2SB = 14 to specify start point of filters for CAN2, the interrupts RX0 and RX1, not work.If i co...

Marco1 by Associate II
  • 1803 Views
  • 3 replies
  • 0 kudos

CSTACK issue with IAP

Posted on February 18, 2016 at 13:37Hi, i'm trying to make an app for my card to introduce IAP (update by ethernet, http in my case)To do this, i'm starting from the example give by stm32 cube STM324x9I_EVAL\Applications\LwIP\LwIP_IAP\EWARM (I test ...

0690X00000605MBQAY.png 0690X00000605MGQAY.png
idealsim by Associate II
  • 2689 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.