2016-02-20 6:31 AM
Hello.
I am using a custom board with STM32F030R8 as my dev platform. I am using Uart2 to configure the board. The RX interrupt is enabled to receive data. i am using PD2 as a GPIO.When i enable peripheral clock to GPIOD, i am not getting uart rx interrupt but uart tx works fine. But when i do not enable the GPIOD peripheral clock everything works fine.I have no idea what is the problem here...Is there something i am missing here?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.