STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 issue

Posted on February 09, 2016 at 23:18Hi,I'm trying to load demo SAI_audio-play from firmware package ''STM32Cube_FW_L4_V1.3.0''  into the flash but I can't, one error send me ==> Error: Flash Download failed  -  Target DLL has been cancelled.My setti...

0690X00000605ZtQAI.png 0690X00000605XUQAY.png 0690X00000605GtQAI.png

STM32F7 and LWIP issue

Posted on March 13, 2016 at 14:38I'm having issues with ethernet on the STM32F7 discovery and nucleo boards.I set up a simple Keil project using STMCube by using selecting the dev board when you create the project. I enabled ETH and LWIP and launche...

kalhana by Associate II
  • 1545 Views
  • 1 replies
  • 0 kudos

STM32F7 SAI/I2S slave issue?

Posted on March 09, 2016 at 13:53Hi, I am working on an application that streams audio from a WAV file on SD card. The core of the code is a hugely simplified version of the ''audio playback and record'' application from the Cube package. Audio outp...

USB cable connected

Posted on March 15, 2016 at 11:18Hi all, I'm working on a device with STM32F205. The MCU does to Stop mode after 15 sec. The device has also USB (VCP) and can be connected to PC. But I don't want MCU goes to Stop mode if USB cable is connected. So m...

donev_g by Associate II
  • 1283 Views
  • 1 replies
  • 0 kudos

Please fix errors in CubeMX FW

Posted on September 03, 2015 at 12:40In cmsis_os.c file -  osPoolDef_t pool_def = {queue_def->queue_sz, queue_def->item_sz}; + osPoolDef_t pool_def = {queue_def->queue_sz, queue_def->item_sz, NULL}; -     else if(ret.value.signals >= 0x80000000) + ...

vromanov by Associate II
  • 3230 Views
  • 6 replies
  • 0 kudos

Cannot combine TIM15/16/17, STM32F030R8

Posted on March 14, 2016 at 06:15Hi, I found an error in RM0360  about TIM15/16/17. It says TIM15 is able to act as a slave timer and triggerred by TIM16 or TIM17 (On page 403, slave timer is TIM15, when chosse ITR2, TIM16 acts as external trigger)....

wangkang by Associate
  • 2926 Views
  • 2 replies
  • 0 kudos

SDRAM and STM32F429 Eval

Posted on June 10, 2014 at 03:33I would like to put my heap in SDRAM on the STM32F429 Eval board but I don't see the options to do so.  I tried the STMCubeMX tools but also did not see any options for this.  I am using the IAR EWARM tools.Thanks

brian2 by Associate II
  • 2281 Views
  • 5 replies
  • 0 kudos

ST32F446 RCC -> CSR PINRSTF allways on

Posted on March 14, 2016 at 17:10Have a question. Nucleo board. in RCC -> CSR  PINRSTF bit is always on. It does not matter what the actual reset source is.  PINRSTF is on + the real reset souce. I clear it using RMVF bit and then generate the reset...

pj by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos

Problem with USART

Posted on March 15, 2016 at 08:31HI, I'm trying to develop a simple communication with my laptop sending just one character, the problem is that I need to send the character more than 5 times for reconogise it in the Discovery board, the code is sim...

vderoc by Associate
  • 1353 Views
  • 2 replies
  • 0 kudos

HAL_SPI_Receive() explanation

Posted on March 09, 2016 at 14:21 Hi, I am examining HAL_SPI_Receive(). At some point it calls return HAL_SPI_TransmitReceive(hspi, pData, pData, Size, Timeout); where pData is the pointer to the rx buffer and Size is...

valerio2 by Associate II
  • 6598 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.