2016-03-15 3:18 AM
Hi all,
I'm working on a device with STM32F205. The MCU does to Stop mode after 15 sec. The device has also USB (VCP) and can be connected to PC. But I don't want MCU goes to Stop mode if USB cable is connected. So my question is, how to find out that USB cabel is connected, which register (bit) from USB core to watch.2016-03-15 6:45 AM
I found the register: ''OTG_FS control and status register (OTG_FS_GOTGCTL)'' and
Bit 19 BSVLD:B-session valid Indicates the device mode transceiver status. 0: B-session is not valid. 1: B-session is valid. In OTG mode, you can use this bit to determine if the device is connected or disconnected. Note: Only accessible in device mode. Bit 18 ASVLD:A-session valid Indicates the host mode transceiver status. 0: A-session is not valid 1: A-session is valid Note: Only accessible in host mode. but these bits have very strange behavior. When I connect PC to the USB (B session) the bits (18 and 19) set to 1 and when disconnect the cable the bits get clear. When connect USB barcode reader (A session) the bits are set and when disconnect the cable they stay set and not get clear any more. Any suggestions?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.