2016-02-06 7:30 PM
Yesterday I upgraded to V4.13.0 which required that I also upgrade to STM32CubeL4 V1.3.0.
Since then, every project that I generate exhibits a couple of problems:1) every reference to RCC_xxx #defines shows up in the IDE as ''Type RCC_xxx could not be resolved''. Same with anything that looks like it could be a system defined preprocessor symbol. The programs compile OK so I think this is an issue with the generated code for the project2) every program starts in debug and, before it gets to the 'main' function, ends up in the ''startup_stm32L476xx.s'' file at some labels called ''Default_Hander:'' and ''Infinite_Loop:'' where the executable code is exactly that - a branch back to the label. I have single stepped through the code form the ''Reset_Handler:'' label and the last statement seems to cause the problem is ''bi __libc_init_array'' in that I cannot step into that function and when I pause the processor I'm at the infinite loop.The console shows:===================================Breakpoint 1, LoopFillZerobss () at C:/Users/Administrator/workspace/Blinky/Drivers/CMSIS/Device/ST/STM32L4xx/Source/Templates/gcc\startup_stm32l476xx.s:114
114 bl __libc_init_array
Program received signal SIGINT, Interrupt.
WWDG_IRQHandler () at C:/Users/Administrator/workspace/Blinky/Drivers/CMSIS/Device/ST/STM32L4xx/Source/Templates/gcc\startup_stm32l476xx.s:134
134 b Infinite_Loop
===========================Have I done something or not done something that has caused this?Susan2016-02-08 2:35 AM
Hi Susan,
Thank you for your feedback. The issue has been reported internally.-Syrine-2016-02-08 9:36 AM
Hello Susan,
Can you please share a .ioc file showing the issue and indicate the toolchain you've selected under project settings. Thank you, Pascale2016-02-08 5:58 PM
I'm at work right now so I'll post the files in a few hours time.
The tool chain was SW4STM32.Susan2016-02-09 1:14 PM
.ioc file attached
Susan ________________ Attachments : Blinky.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htq3&d=%2Fa%2F0X0000000aXZ%2Fkd2sVbdCoMlbwLJHf.6upey0514EtNkxEVCg9aRCeBM&asPdf=false2016-02-11 1:53 AM
Hello Susan,
We don't reproduce your issue. Can you please ensure your SystemWorkbench installation is up to date? Can you also check that under STM32CubeMX Project Settings menu, you have changed the IDE to SW4STM32 (loading the project does not load the configuration formerly done on the project settings window) Best regards2016-02-12 9:08 PM
Thank you for looking into this.
I have attached two files: - a description of the steps I've taken - a zip file of the workspace directory tree (after it was initially cleared) Perhaps the additional information might help. Susan ________________ Attachments : STM32Cube_Problem_Description.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htq8&d=%2Fa%2F0X0000000aXc%2FqvxlHrN3Uao1aamPa3.QuZ1fqkNXd4nDCF7eM2iFDho&asPdf=falseworkspace.7z : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtqD&d=%2Fa%2F0X0000000aXd%2FH5sxk9Do3awoh_N3fhUoGAxrramW9Wbd0JIQnC6ead0&asPdf=false2016-02-15 1:52 AM
Can
I also
will report
here
a small
problem
?
Tab
''Help-> Install New Libraries''
now becomes
larger in
height
than before
(>
800
pixels
)
and
a Netbook
PCfor example,
is no longer possible
to get
on this tab
to the lower
buttons
.
If possible
, reduce
as before
(
<=768
)
in height.
And in general -
I
was happy with everything
in this program.
Compared with the same
software
from the
''
competition
''(
the letter 'M'
begins
name ofthis company
) - is like ''Heaven and Earth''
!!!
I recently
(
3 months
)
transferred
to the controllers
of
/
!!!God bless you
and thank you
!
2016-02-21 6:22 PM
Is there more information that is required for this to be looked at?
At the moment, I can't make any progress as everything I try ends up at this tight loop.Susan2016-02-21 8:57 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.