STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to program when in stop mode

Posted on March 22, 2016 at 18:41I'm unable to program a STM32 using the STLink2 when the micro has firmware running that puts it into stop mode.I've played with the reset sequence settings in Keil but none of them solve my problem.Does anyone know ...

bluscape by Associate III
  • 2222 Views
  • 3 replies
  • 0 kudos

STM32F4 Dual ADC Reg Sim Mode with DMA

Posted on March 21, 2016 at 18:02 Hello, I want to read ADC1 CH0 and ADC2 CH1 in dual regular simultaneous mode and buffer it in DMA. I want to send the ADC values via UART to my PC and read them from the COM Port. When I start the program n...

LTDC is DMA?

Posted on March 23, 2016 at 08:27Hi ,Can any one tell me,Whether LTDC is DMA or not?LTDC is basically working as blocking or non blocking?By Tamilselvan

Confused by STM32L4 datasheet max SPI clock frequencies

Posted on March 22, 2016 at 20:10I'd like to use an STM32L4 in a project where I am interfacing with a 1-MSPS, 16-bit SPI ADC (LTC2378-16).  Obviously the SPI clock has to be > 16 MHz to run this at full speed.  However, for best performance the clo...

mhaun by Associate II
  • 3004 Views
  • 2 replies
  • 0 kudos

sdio dma--emmc

Posted on March 21, 2016 at 10:13Hi i am using f4 and it works with the polling method. But it doesnot work on DMA.. i am getting SDIO_IT_RXOVERR error. Can anyone  help me ?

arunease by Associate II
  • 976 Views
  • 1 replies
  • 0 kudos

32F429IDISCOVERY

Posted on March 22, 2016 at 18:20Does this kit require a BDM to program the  STM32F429ZIT6.  Or does it work through the USB? I am new to ST products and what kind of tools do I need to use to program the device.

STM32F103ZE, debugging imprecise bus fault

Posted on March 17, 2016 at 13:43Hi,I am still debugging a bus fault for almost 4 months.I read about DISDEFWBUF flag from ACTLR, then, i check the register window. what I have there is ACR register which contains DISDEFWBUF bit.I tried to set that ...

Stbymode and RTC on STM32F205

Posted on March 20, 2016 at 13:39helloi am working on an stm32f205 project. before adding the RTC part , the stbby modeworks fine.when i added the RTC part   (i tested it and it works fine), but my system dont want toget in stby mode. the RTC wakeup...

websat13 by Associate II
  • 3566 Views
  • 8 replies
  • 0 kudos

CubeMX USART bug on PB6 Pin of STM32F7 Disco

Posted on March 19, 2016 at 04:02PB6 pinned as USART1 TX its wrong in software, the correct option is also available (PA9), but the PB6 one should be deleted, is used by default if you don't configure it manually. #bug #tx #usart1

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.