2016-03-18 8:02 PM
PB6 pinned as USART1 TX its wrong in software, the correct option is also available (PA9), but the PB6 one should be deleted, is used by default if you don't configure it manually.
#bug #tx #usart12016-03-21 5:18 AM
Hi noto.federico,
I have checked this using the last version of CubeMx (4.1), and I do not see the issue that you havementionned; every thing goes well and PA9 is well selected by default as USART_Tx. So Maybe you have used an old version of CubeMx ? Try with this last version of STM32CubeMx (4.1
) and hopefully your issue will disappear. I have attached the .ioc of th test project That I have used. -Hannibal- ________________ Attachments : Pin_USART_TX_PB6_and_P19_together.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htjv&d=%2Fa%2F0X0000000aWQ%2FlRi826x77RyaHcnOdgWI4PKX3A9anNrKf82KFttT6tw&asPdf=false2016-03-22 2:28 PM
Why is USART1_TX in PB6 Pin? (I'm using 4.14.0 Version) , yes, now USART1_TX by default assing the correct pins.
2016-03-23 4:19 AM
Hi noto.federico,
Yes, it is selected by default PA9, but you can remap it to PB6. Take a look to both ( Table 10 and Table 12) to see the pin definition and the associated possible alternate functions. IT is nice to hear that everythig is fixed now for you. -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.