2016-03-22 10:20 AM
Does this kit require a BDM to program the
STM32F429ZIT6. Or does it work through the USB?
I am new to ST products and what kind of tools do I need to use to program the device.2016-03-23 4:22 AM
Hi morley.daniel,
Welcome to STM32 community :)I'd highly recommend you to have a look to these two documents, they provide guidelines to novice users on how to build and run a sample application and to create and build their own application around the STM32F429 Discovery.•http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00097320.pdf
•http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00092920.pdf
Also I recommend you to download thehttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber
which is a graphical software configuration tool that allows generating C initialization code using graphical wizards.-Syrine-2016-03-23 6:05 AM
The DISCO board includes an SWD (single wire debug, like jtag, fewer pins) debugger, ST-LINK, provided by the F103 part on the board. This connects via the primary USB (mini), the target USB (micro).
The DISC1 model support mbed, and a virtual serial port.The ST-LINK debugger is supported by Keil, IAR, etc.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.