STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC and reset problem

Posted on March 31, 2016 at 14:20Hi to all, I encounterd a problem using Real Time Clock. After I initilaized it, everything seems to work, but when I reset MCU it stops and I can restart my board only powering it off and then on again. Hereafter th...

Vbat circuitry

Posted on April 01, 2016 at 07:06Hi. We would like to store some data in a backup registers using supercap as an additional power supply. Do you have maybe any recommendation for the circuitry around the supercap? Or maybe an example of it? It shoul...

matic by Associate III
  • 982 Views
  • 1 replies
  • 0 kudos

watchdog

Posted on April 01, 2016 at 11:51Hi i have implemented watchdog on f429. i have two applications on flash , one is  bootloader and other one is an application program . i have implemented the watchdog on bootloader and also jump function from bootl...

arunease by Associate II
  • 1161 Views
  • 1 replies
  • 0 kudos

stm32f1 RTC problem in HAL

Posted on March 31, 2016 at 16:26Why HAL library do not solve RTC problems?RTC counter reset after a day.how can I save My Date ?RTC counter reset After power up.

CUBEMX -> code -> add TSL Lib something is wrong

Posted on March 30, 2016 at 11:11 hi,  CUBEMX made simple code which works, than i add Touch driver1.4.4 and get errors, why this two  do not compatiable ?  - KEIL , comman line:   USE_HAL_DRIVER, STM32L152xB. compile : - '' GR1 has already been ...

enmirc by Associate II
  • 2033 Views
  • 5 replies
  • 0 kudos

Touch Sensing on STM32F0

Posted on June 15, 2012 at 13:27Hi, it is stated in STM32F051 RM that the MCU was designed to work with STM32 TSL. I attempted to build a prject with the TSL, however it supports only STM32L and would not build saying that ''instruction is unsupport...

eltar by Associate III
  • 5698 Views
  • 16 replies
  • 0 kudos

[Novice]Having problem with basic project

Posted on October 14, 2015 at 14:51 Good day everyone. I try to run example from Eclipse (blinking led) onSTM32F051R8T6. But nothing heppend. Could anyone give me advice? Thanks. This is server log: Last login: Tue Oct 13 23:23:12 o...

dikhnot by Associate II
  • 3214 Views
  • 6 replies
  • 0 kudos

IWDG disbale steps for STM32F2xx/STM32F4xx

Posted on March 28, 2016 at 16:05I learned that, to enable IWDG we need to write 0xCCCC to IWDG->KR register.I have a situation where I enable IWDG peripheral in bootaloder image and I want to disable IWDG in Application.Can anyone help me to unders...

vinay2 by Associate
  • 1313 Views
  • 2 replies
  • 0 kudos

Converting TFT Library from arduino to use with STM32F4

Posted on March 31, 2016 at 18:32Hello there, I've recently got a new 1.8 TFT LCD Module with seems to be using S6D02A1 Driver chip from samsung.I found this library for arduino https://github.com/sumotoy/TFT_S6D02A1 ... After many attemps I was una...

monta by Associate II
  • 798 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.