STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generation of odd freq with Timer Peripheral

Posted on April 25, 2016 at 14:20Hi , I want to generate signal equal to 2.048MHz for audio codec IC which need to be very precise . Right now I have configured TIM8 CHN3 with per-scaler = 0 and period = 40 and timer peripheral clock is around 84 MH...

ucLinux USB Gadget support

Posted on May 13, 2016 at 14:49Hi All,I'm using Emcraft's uCLinux deposit. For host-side USB support on the STM32F7 this uses the dwc2 driver. However when I configure the kernel to have gadget support it fails to build.I've read this post (https://...

APB1-TIM Inputcapture with DMA1 not working [solved]

Posted on May 13, 2016 at 15:49 Hello, I tried to use the TIM2/3/4/5 Input-Capture with DMA (''TIM_DMA_CC1'') to trigger a DMA-Transfer (this writes to a GPIO-Port for parallel Data-transmission) but it just Work with DMA2, not DMA1. ...

andre23 by Associate II
  • 2035 Views
  • 4 replies
  • 0 kudos

stm32f429 sdio bootloader

Posted on May 13, 2016 at 15:42Hi,I want to update firmware by using the sd card with my stm32f429 mcu. I will connect the sd card to mcu sdio pins ( 1 bit only) , so i will not use spi port for sd card. I just want to learn whether it is possible t...

er3481 by Senior
  • 1057 Views
  • 1 replies
  • 0 kudos

STm32CubeMX bug : CAN1 wrong configuration

Posted on March 02, 2016 at 11:57 Hi, I tried to configure my STm32F107 using the ''Cube'' to use the CAN1 and user ledsand I found a bug. This is the initialization code generated by the ''Cube'': void HAL_CAN_MspInit(CAN...

b2399 by Associate II
  • 1798 Views
  • 4 replies
  • 0 kudos

STM32Java webpage missing

Posted on May 13, 2016 at 09:56Searching for STM32Java on the new st web yields the following link: http://www2.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-ides/stm32-java.htm...

SPI NSS cannot change automatically

Posted on May 05, 2016 at 17:07Hi, If I configure NSS as hardware management, it it controlled by the SPI peripheral. However, from the manual, the NSS is low when the SPI is enabled, and NSS is changed to high only when SPI is disabled.I think it i...

wenbin by Associate II
  • 2023 Views
  • 4 replies
  • 0 kudos

AN2824, Optimised I2C - Repeated Start Condition ?

Posted on May 11, 2016 at 12:30The Application Note doesn't seem to consider the case of a Repeated Start Condition.Are there any special considerations?Although the App Note specifically addresses STM32F10x, I am actually using an STM32F411 - See: ...

F107 USB OTG as a device only

Posted on May 05, 2016 at 19:13Folks, I have code for using the F103's USB device port as a virtual com port. Does anyone know: 1. Could I use that ''as is'' on the F107's OTG port. I only ever want to use it as a device. 2. Do I really have to hav...

DiBosco by Senior II
  • 1068 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.