STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with uint64_t and EXTI Callback function

Posted on May 11, 2016 at 15:43Hello, I use the HAL EXTI callback function on an STM32F411 and have made the following strange experience: When changing data types from float to uint64_t for Efficiency in another callback function (actually from DMA...

herbert by Associate III
  • 2915 Views
  • 11 replies
  • 0 kudos

SPL USB HID get idle status

Posted on May 06, 2016 at 18:58Hello, I am working on project where i need to send hid reports to android phone. I know how to send data, but i need to send empty message to unpress all buttons. How can i do that, how can i know, when message is sen...

Two Virtual COM Ports

Posted on May 11, 2016 at 13:01Hello. I made a code to send and receive data via USB bus based on the CubeMX CDC (Virtual COM Port).Now I can emulate one virtual COM Port with STM32F407VGTx Discovery Board, but actually I'm thinking if I can emulate...

Getting the TimeStamp betterway in ms in STM32F4

Posted on May 09, 2016 at 06:15How can we get the timestamp information in a better way in ms - using systick configured @1ms and calling HAL_GetTick() to get the time in ms or using RTC? #systick #priority #!stm32f4-!stm32f401-!rtc #stm32f4

darla14 by Senior
  • 6922 Views
  • 10 replies
  • 0 kudos

CubeMX examples are not examples

Posted on May 10, 2016 at 21:08The examples in the CubeMX repository do not use CubeMX to generate init code.  This means that they may be a little useful for showing examples of on-chip and on-board peripherals working, but give little assistance i...

SDRAM memory bandwidth

Posted on May 11, 2016 at 10:51Hello! Can anybody explain how to calculate SDRAM memory bandwidth, please? One example.

Measure RMS and frequency with stm32f405

Posted on May 10, 2016 at 15:21I have to measure current and voltage rms as well as frequency for three phase sinusoidal. Is there an application note about measuring rms and/or frequency with the stm32f4 series? I 'm checking the specification and ...

zdravko by Associate II
  • 1891 Views
  • 2 replies
  • 0 kudos

CubeMX and CubeMX Example programs

Posted on May 08, 2016 at 11:07It is far from intuitive how to re-create the functionality of the CubeMX example or Application example programs using CubeMX. So why are they part of the CubeMX repository environment.  For example, I am currently tr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.