STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem in PWM output

Posted on May 09, 2016 at 19:30Hello,I m configuring STM32F303xx processor for driving BLDC motor driver IC.I have read the datasheet of the same processor.From that i found that we can use TIM1 in Combined PWM mode (for driving 3-Phase BLDC motor)....

SS.Sagar by Associate III
  • 1332 Views
  • 3 replies
  • 0 kudos

STM32F4xx Internal RTC not Updating when Power is Off.

Posted on May 11, 2016 at 12:43I am using Internal RTC of STM32F411RCT6. It's working Perfectly but I cant update it when Power is off. I want to say that i have connected 3 v DC supply with VBAT pin and Run my RTC program, it works good but when i ...

jay1991 by Associate II
  • 6456 Views
  • 14 replies
  • 0 kudos

Severe issues with the new ST website

Posted on April 12, 2016 at 07:30Hi,I do not want to be argumentative, but the new ST website is doing it wrong. Again.Actually, it's impossible to download several softwares, tools or even datasheets in reliably manner. For example, if you go to th...

carmine by Associate II
  • 6604 Views
  • 15 replies
  • 0 kudos

USART2 (PA2, PA3) in polling mode

Posted on May 12, 2016 at 07:17The original post was too long to process during our migration. Please click on the attachment to read the original post.

phd by Associate
  • 1959 Views
  • 3 replies
  • 0 kudos

run program at address other than 0x8000000

Posted on May 13, 2016 at 09:10I have STM32L4, and I want build a program run at address like 0x08080000. My env is uVision5, and I set the 1ROM1 address to 0x08080000 in uVision. I use fromelf command to generate the bin file from axf file and load...

jiangpen by Associate II
  • 4634 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.