STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RBT6 SOFTWARE UART

Posted on May 30, 2016 at 08:55I am working on stm32f103rbt6 controller, I require 4 UARTs but this controller having  only 3 UARTs so I am trying for software UART,I have attached my program file here, can anyone help me for writting code.         ...

Reading ADC lower amplitude values

Posted on May 31, 2016 at 13:38Good day,I am trying to read sinus from audio line in.But I see that I could only read higher value of my amplitude, here is the example:http://s33.postimg.org/i5ew1ozgf/sin.jpgMy source code:#define IO_PIN       GPIO_...

hitsumen by Associate II
  • 1398 Views
  • 1 replies
  • 0 kudos

I need some help to save stm32f407vgt6

Posted on May 31, 2016 at 05:59Hello everyone! I use to stm32f4-discovery kit. because I was careless, I used PB2( BOOT 1) as GPIO( external intterup line 2). and now I can't load code for chip. what i can do to save it? Thanks for read !!!

quocanh by Associate
  • 1288 Views
  • 2 replies
  • 0 kudos

Problem with set priority in STM32F429ZI.

Posted on May 31, 2016 at 11:02#include < main.h > #define Led_Green GPIO_Pin_13 #define Led_Red GPIO_Pin_14 void LED_Config(void) { GPIO_InitTypeDef GPIO_Init_Var={0}; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); GPIO_Init_Var.GPIO_Pin = G...

UART / USART baud rate

Posted on May 27, 2016 at 14:57Is it possible to use baud rate divisor less than 1? i.e. 1/16 - USART_BRR = 0x01I did not find any information about it in STM32F4 RFM.  #uart-usart-baud

aseris by Associate II
  • 2004 Views
  • 6 replies
  • 0 kudos

zany idea: getting more bits resolution out of the ADC

Posted on May 30, 2016 at 16:28The STM32F7 onboard DAC is only 12 bits.  I only need mono audio input.  Suppose I drive the left ADC input directly and the right from an op amp gain stage of say x16 and then combine the lowest 4 bits of R with left-...

dennis by Associate II
  • 4047 Views
  • 3 replies
  • 0 kudos

HASH_RNG_IRQn vs RNG_IRQn in STM32F20x headers

Posted on May 31, 2016 at 11:19Hello, even the V2.1.1 headers for the F2 family still define HASH_RNG_IRQn for the F20x devices that don't have the crypto feature. The F20x header should use RNG_IRQn. Regards #stm32f20x #headers

EXTI_IRQ with USerButton problem

Posted on October 31, 2015 at 15:42 Hello there! I have designed a custom board, and what I'd like to do is that when I press the UserButton, a LED lights up.Now, my button is connected to PC0 pin on my STM32F429 controller, and the LED i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.