2016-05-31 4:38 AM
Good day,
I am trying to read sinus from audio line in.But I see that I could only read higher value of my amplitude, here is the example:http://s33.postimg.org/i5ew1ozgf/sin.jpgMy source code:#define IO_PIN GPIO_Pin_5#define IO_PORT GPIOC#define IO_PORT_CLK RCC_AHB1Periph_GPIOC#define ADC_CLK RCC_APB2Periph_ADC1#define ADC_NUM ADC1#define ADC_CHANNEL ADC_Channel_15void ADC_start_test(void){ ADC_SoftwareStartConv(ADC_NUM);}void ADC_init_test(void){GPIO_InitTypeDef GPIO_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
ADC_InitTypeDef ADC_InitStructure; /* Enable peripheral clocks */ RCC_AHB1PeriphClockCmd(IO_PORT_CLK, ENABLE); RCC_APB2PeriphClockCmd(ADC_CLK, ENABLE); /* Configure ADC Channel 10 pin as analog input */ GPIO_InitStructure.GPIO_Pin = IO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* ADC Common configuration *************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_DualMode_RegSimult_InjecSimult; // APB2 clock is half the 168Mhz system clock (i.e. 84Mhz), // so with a div by 8, ADC PCLK would be 10.5Mhz. // F4 datasheet says ADC clock freq should be 0.6Mhz - 30Mhz for Vdda=3.3V ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div8; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; //TwoSamplingDelay is only used in dual and triple modes) ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 regular channel 10 to 15 configuration ************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; // 1 Channel ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; // Conversions Triggered ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; // Manual ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T2_TRGO; //Unused for manual? ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); //The sample time is how long the input is sampled before the conversion is done. //Since PCLK is 10.5Mhz, 144 cycles is about 13.7uS and the DAC output rate is //running manually off a 44Khz timer interrupt (22uS), we should be fine //(once conversion starts, it takes about 16 cycles) ADC_RegularChannelConfig(ADC_NUM, ADC_CHANNEL, 1, ADC_SampleTime_144Cycles); /* Enable ADC1 */ ADC_Cmd(ADC_NUM, ENABLE); ADC_start_test();}//Get ADC value if the ADC is ready//Returns value if successful, -1 if ADC wasn't done yetuint16_t ADC_get_test(void){ //HACK - TESTING while (ADC_GetSoftwareStartConvStatus(ADC_NUM) != RESET) ; //HACK - TESTING return (ADC_GetSoftwareStartConvStatus(ADC_NUM) == RESET) ? ADC_GetConversionValue(ADC_NUM) : -1;}
2016-05-31 5:41 AM
What am I looking at?
The ADC isn't going to work with negative voltages, and likely violates the specs.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.