STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Install u-boot on stm32f4 discovery board

Posted on June 15, 2016 at 17:43Hello guys, I'm trying to install u-boot on my development board STM32F407 . After loading the binary image, the UART1 interface does not work . I'm using the version available from the website emcraft for the board S...

rs23 by Associate II
  • 1282 Views
  • 1 replies
  • 0 kudos

HAL bug - array overflow in HAL_RCC_GetSysClockFreq()

Posted on June 10, 2016 at 17:23The purpose of this post is to save other developers the time I have spent tracking this down. Bear with me on this - its messy. Line 1108, of stm32f1xx_hal_rcc.c is  if (pllmul == aPLLMULFactorTable[(uint32_t)(RCC_...

UART DMA INT is not working

Posted on June 16, 2016 at 10:30 Hi, I'm facing a strange problem with UART DMA int in a FreeRTOS-based project. When I call the DMA setup function (below) from a given FreeRTOS task, it works just fine and the ISR is executed. However...

0690X00000605PtQAI.png
asaad by Associate
  • 783 Views
  • 0 replies
  • 0 kudos

GPIO speed settings

Posted on June 16, 2016 at 08:28Hi. I would like to ask if speed setting of a pin in GPIO->OSPEEDR register is relevant also if a pin is configured in input/alternate mode? Or is this setting relevant only for output mode? I am asking specifically f...

matic by Associate III
  • 2392 Views
  • 1 replies
  • 0 kudos

F103, F401, F407 USB code replace

Posted on June 15, 2016 at 22:41Hi. I found this project : https://github.com/jpbarraca/LogicAlNucleo This code is for NucleoF401RE board, which costs about $20. I have cheap chinese board with STM32F103C8T6, resources looks enought, but code not w...

tuxcnc by Associate
  • 2274 Views
  • 3 replies
  • 0 kudos

Problems with cube implementation of get/set for RTC

Posted on June 16, 2016 at 00:49The cube hal code for getting and setting the time/date have some significant issues -- at the very least the documentation is woefully inadequate.The fundamental issue is that setting (getting) time/date requires two...

Specifications for the F429 DISCO LCD available?

Posted on October 10, 2013 at 15:03Hello, are specifications and command descriptions for the LCD Display on the F429 Disco available? It is a SF-TC240T-9370-T type display. Google only brings up information for the SF-TC240T-9229A2-T that doesn't h...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.