STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F072xx USB Hardware

Posted on June 14, 2016 at 22:54Hello,Where can I find info on hardware needed to run USB to my STM32F072CB?  I found the reference design and read hardware getting started.  Neither specify how to get USB levels down from 5V to uC VDD.  5V can't go...

jezell by Associate
  • 2179 Views
  • 4 replies
  • 0 kudos

three_input_capture_xor_gate reading on stm32f429i_discovery

Posted on June 15, 2016 at 18:33Hello, We would like to read hal sensor outputs(H1,H2,H3) of bldc motor by xor gate of TIM4 channels. We select SLAVE mode for RESET MODE to read number of squarewave of xor gate outputs of TIMER4 but it does not wor...

bhakan by Associate II
  • 1301 Views
  • 1 replies
  • 0 kudos

Install u-boot on stm32f4 discovery board

Posted on June 15, 2016 at 17:44Hello guys, I'm trying to install u-boot on my development board STM32F407 . After loading the binary image, the UART1 interface does not work . I'm using the version available from the website emcraft for the board S...

rs23 by Associate II
  • 973 Views
  • 1 replies
  • 0 kudos

replace STM32F405 with STM32F415

Posted on June 14, 2016 at 21:16Hi all,I have a design based on the  STM32F405  working, I would now like to try out the  STM32F415, is it the case that  on the hardware side I can just replace the  STM32F405  on PCB with the  STM32F415 - given that...

kweisi50 by Associate II
  • 964 Views
  • 2 replies
  • 0 kudos

STM32 part numbering ''Software option''?

Posted on June 15, 2016 at 08:26Hi, In STM32F105xx datasheet, in part numbering section, it has an option named ''Software option'', and it has two options: internal code or black. What does it mean? #!stm32 #part-numbering

0690X00000605PoQAI.png

Limitation with Read protection active with stm32f105rb

Posted on June 15, 2016 at 16:03Hi, I made a loader with usb STM32F105 and working properly. When I active the read protection bit, the loader not erase the pages. The security bit is on and of course, I can not debug and find where is the problem. ...

Marco1 by Associate II
  • 677 Views
  • 1 replies
  • 0 kudos

Problem with RTC and LPTIM interrupt in STOP Mode

Posted on June 14, 2016 at 16:31I am using NUCLEO-L11K4 board for my low power monitor project. I want to wake up board periodically every 5 minutes and send message center. Meanwhile i want to wake up the board with external interrupt in the case o...

Receiving register address byte with STM32F407 as I2C slave

Posted on June 15, 2016 at 00:58 Hi I have written a small proeject where I have set up an STM32F407 on a discovery board as an I2C slave, and I'm pleased to say that it is mostly working. The problem I have is that when I send the follo...

AJE by Associate II
  • 1091 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.