STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need help to get started with bootloader program

Posted on June 29, 2016 at 19:11I've read a few documentations from STMicro but still not sure what the actual steps to do a proper bootloading.  Here is what I understand so far.1. First the bootloader firmware is already on the uC so I don't have ...

Vu.Andy by Associate III
  • 2507 Views
  • 5 replies
  • 0 kudos

Question on USART interrupt and when it occurs

Posted on July 01, 2016 at 20:26For example, if I call the function HAL_UART_Receive_IT() with a buffer size of 16. When will the interrupt be triggered? Is it when all 16 bytes are filled up?  Or when the Usart finished received all the data? Will ...

Vu.Andy by Associate III
  • 1019 Views
  • 1 replies
  • 0 kudos

Internal Clocking and Sample Rate on STM32F4 ADC

Posted on July 01, 2016 at 18:59Hi, I was wondering how the built in ADC on the STM32F4 was clocked, and how I could go about checking it's clock frequency. I know that the sample rate is configured by dividing the clock (e.g. ADC_SampleTime_480Cyc...

epalaima by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

Problem with STM32F446FE and STM32 MAT/TARGET

Posted on June 24, 2016 at 13:26Hello everyone, I am trying to program the Nucle STM32F446FE using the STM32 MAT/TARGET and a Simulink Model, but when I build it, Simulink doen't continue with the process, blocking itself. I have downloaded the late...

julio by Associate II
  • 2089 Views
  • 4 replies
  • 0 kudos

STM32CubeMX + FatFS - Keil works, TrueStudio not

Posted on June 30, 2016 at 13:02 Hello my friends, I am new to FatFs and I want to write something on the SD-Card. I initialize SDIO and FatFs over STM32CubeMX. I am using the STM32F4 Discovery and the Baseboard which has a SD-Conne...

CRC multithreading

Posted on July 01, 2016 at 10:45Good day. In my program i use CAN interface. I send and receive messages (consist of few CAN packs) with crc. When i receive the CAN pack i put it into buffer and when the message complete i calculate it crc.Transm...

STM32 F0 - leaving dfu mode

Posted on June 30, 2016 at 16:49Hello,I have a board with F072, BOOT 0 pin is low.When I use ''Leave DFU mode'' (Dfuse Demo 3.0.5), board left DFU mode but the application is not restarted.  Content of flash memory at address 0x00000000 and at addre...

SPI slave TX FIFO clearing....

Posted on June 30, 2016 at 16:20I have an SPI slave. The master may request data at a faster pace than I can handle in software, so I've set up DMA. I've prepared a buffer etc. Now after one transfer, I get an interrupt of the DMA having finished (i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.