2016-07-01 9:59 AM
Hi, I was wondering how the built in ADC on the STM32F4 was clocked, and how I could go about checking it's clock frequency.
I know that the sample rate is configured by dividing the clock (e.g.ADC_SampleTime_480Cycles).
So I'd like to figure out the clock rate and thereby be able to set a specific sample rate.
#clock #adc #sampling-rate2016-07-01 11:45 AM
Ok, so that time plus the 12 cycles for a 12-bit conversion. The clock going to the ADC is from the APB/AHB to which it is attached, that is divided down by the prescaler you can chosen for the ADC. So cycles of the clock coming out of the scaler/divider. So if that is 14 MHz, then 492 cycles of that.
If you want samples to occur at a specific clock or sample rate, you'd want to setup a timer and use that to trigger the start of the conversion. The converted value can then be services by an EOC interrupt, or by a DMA transfer to a memory array. If sample more than one channel you will need to use DMAWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.