How to implement UART receive with unfixed data size?
Posted on July 01, 2016 at 07:39Hello all,I use STM32F303VC and plant to use UART to receive data, but the receive size of data are different. Does anyone know how to implement it?Thanks
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on July 01, 2016 at 07:39Hello all,I use STM32F303VC and plant to use UART to receive data, but the receive size of data are different. Does anyone know how to implement it?Thanks
Posted on June 25, 2016 at 09:20Hello, I'm looking for information about the circuits to add to a STM32F7 Nucleo board to build an operational SPDIF output. I tried to find the information in the STM32 reference document, but could not find the inf...
Posted on June 28, 2016 at 21:11I have a STM32F4 Discovery board. I have GDB connected to OpenOCD and when I run my program on GDB it executes perfectly. When I disconnect the board and program it via ST-Link nothing happens. I tried and older progr...
Posted on February 06, 2016 at 18:06 I am using STM32F407VGT-6 chips. I use the DMA2 Stream0 with the ADC1 to read analog values. On two of my Boards, the code is working fine and I am not having any problems. On a third Board I programm...
Posted on June 24, 2016 at 09:24Hello, I'm looking for information about the circuits to add to a STM32F7 Nucleo board to build an operational SPDIF output. I tried to find the information in the STM32 reference document, but could not find the inf...
Posted on June 30, 2016 at 21:57I plan to use the STM32F40x TIM1 CH1 (PA8) to produce a varying PWM signal. The base frequency is set, say 1 MHz. I need to use DMA to change the PWM duty cycle on every iteration. I know this can be done by aiming...
Posted on June 30, 2016 at 16:43Hello,I'm navigating trough STM32L052 documents but could not find any information on specific IRQ numbers besides the ''stm32l052xx.h'' from Cube L0. Also, connections between peripherals, EXTI and the interrupt cont...
Posted on January 02, 2012 at 04:06I am using STM32F103 MPU.I set the board as SPI Slave and uses DMA to receive and send data.Most of time Command comes from Master and Slave responses.So I made code to wait for receiving Command from Master. Once ...
Posted on June 28, 2016 at 17:39I wish to transfer a large array of data to 8 output pins that are all on the same port. E.g. a 500 element 8bit array where each bit of each element represents the pin status.So 500 independent transfers to the port ...
Posted on June 30, 2016 at 12:38hi i wanna connect stm32f407discovery board to stm32f429 via uart communication. how can I calculate the closest baud rate to 5Mbps for these 2 board? I use following cod and it work but I want to be sure about minimu...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.