STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt conflict on PB11 PC11 pins

Posted on July 08, 2016 at 15:14Hi,I'm working on stm32f410RB Nucleo board and I have to set interrupt on pins PB11 and PC11 but on CubeMX project setting one pin exclude the other one interrupt, why?I have to configure it manually or is an hardware...

redcrow by Associate
  • 1583 Views
  • 2 replies
  • 0 kudos

STM32L152D ADC with DMA not working

Posted on July 08, 2016 at 11:49 Hello everyone, I am implementing some code forSTM32L152D-Eval Board using CubeMX; I set up one ADC channel (on pin PF10) with DMA transfer, but I don't get any data after starting the DMA: HAL_ADC_...

anio1491 by Associate II
  • 1303 Views
  • 1 replies
  • 0 kudos

Stm32f4 beginner qustions

Posted on July 05, 2016 at 07:54Hi, I am new to stm32f4 and just started picking up some basic skills on it. Hope you guys help me answer my doubts even though the questions I ask are very basic but it will really help me out. 1. Why do we need a ti...

what's the initial stack address of stm32?

Posted on July 08, 2016 at 09:44 Hi guys: I've alredy checked the .map file. I found the two STACK 0x2000c170 Section 2304 startup_stm32f10x_cl.o(STACK) __initial_sp 0x2000ca70 Data 0 startup_stm32f10x_cl.o(STACK) And i...

BeMercy by Associate II
  • 1305 Views
  • 1 replies
  • 0 kudos

Urgent - Keil uVision code limit reached

Posted on July 08, 2016 at 01:28Hi all,I'm a student, mainly using Keil uVision to program an STM32F4 for my own quadcopter flight controller. I'm also nearing the end of a small contract using the same MCU and uVision software.Last week I reached t...

max239955 by Associate II
  • 5653 Views
  • 5 replies
  • 0 kudos

Communication between two stm32l031k6 (lib STM32cubemx)

Posted on July 07, 2016 at 10:50 Hello xD, I want to communicate with two STM32L031K6 in SPI with the library HAL for STM32CubeMX. I configure a Master with emission interruption and the other in slave reception with interruption. and I connec...

ibrahim by Associate II
  • 1235 Views
  • 1 replies
  • 0 kudos

ADC pin Current Draw

Posted on July 08, 2016 at 09:13I am looking for the typical as well as the maximum value of ADC pin current draw while it is sampling. My micro is a STM32F103.Many thanks. #adc #adc-pin-current-draw

STM32L4 - New packages planned?

Posted on May 18, 2015 at 19:26Hello First of all, congratulation for the power efficiency of the ''new'' STM32F411, at low speed it's actually more efficient than a STM32F0, impressive. But I'm missing one important feature, it hasn't touch sensor ...

Tantalum by Associate II
  • 4276 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.