2016-07-19 3:51 PM
The Memory Protection Unit (MPU) is a feature that is only implemented in some members of the STM32F1xx family.
Is there a simple table which I can peruse to determine which members have the MPU, and which don't have this feature?2016-07-20 1:36 AM
Hi,
You should refer to the corresponding device datasheet to see if the MPU feature is present in the STM32 type you are using. You can refer to this , it can help you in section 4.2 Memory protection unit (MPU)Regards2016-07-20 5:02 AM
2016-07-20 6:35 AM
Top post responses...
How many F1 chips do you need to use? Can you use other critical parameters to pare down the list a bit?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.