STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

uart baud rate supported by internal 48Mhz oscillator

Posted on July 29, 2016 at 04:52I am using this STM32F0 MCU http://www.st.com/content/ccc/resource/technical/document/datasheet/0a/d2/ad/ae/d4/04/44/e3/DM00098745.pdf/files/DM00098745.pdf/jcr:content/translations/en.DM00098745.pdfIt has an internal ...

STM32F746 USB problem

Posted on July 27, 2016 at 18:51Dear ST,I have a problem letting my STM32F746 (144 pin) USB CDC (device) work properly, every time I connect it to the PC I got this message:  (The device cannot start ... code10)This is the steps I did to get this pr...

Sw or Damaged Board?

Posted on July 26, 2016 at 21:09Hello all, I've recently acquired an STM32 Nucleo-F103RB evalutation board. I've used STM32 cube to generate a sample program for both free versions of atollic true studio and IAR for ARM. When trying to program/Debug...

0690X00000605baQAA.png 0690X00000605YmQAI.png

STM32F4 LTDC - scan lines

Posted on July 29, 2016 at 13:19Hi All, My hardware is custom STM32F429 board with 7'' TFT. Display has no U/D or R/L display mode select pin. I don't see datasheet LTDC registers to configure scanning order. Actually i do it manually in software, p...

prog by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

STM32F030 dectected as STM32F09xx

Posted on July 28, 2016 at 16:51Can anyone help me.I am trying to bring up the stm32f030 chip. but the STM-link program is detecting it as a stm32f09xx .

twan by Associate
  • 1137 Views
  • 2 replies
  • 0 kudos

STM32 gpio help

Posted on July 28, 2016 at 21:19 I'm new to arm programming, I'm teaching myself with the STM32 specifically the STM32F030x6. To start myself off with any new mcu arch, I write a simple as ever code that would make one of the gpio pins go high...

TIM_OCMODE_PWM1 not selectable in STM32CubeMX

Posted on July 27, 2016 at 17:58Hi there,I just want to generate a simple Pulse Width Modulation with the STM32F303RE with Timer 1 / Output Compare Channel 3.But I can not select the desired mode TIM_OCMODE_PWM1 for sConfigOC.OCMode.Do I have to con...

Doxygen has trouble with ST CubeMX generated HAL code

Posted on July 28, 2016 at 19:03Has anyone tried to run Doxygen over generated code from ST CubeMX? I tried to run it and HAL driver function's comments cannot be extracted and correctly displayed. See the attached picture. It can generate the link ...

yfang by Associate
  • 1127 Views
  • 0 replies
  • 0 kudos

Wrong value of Duty Cycle value of PWM Input Capture

Posted on July 28, 2016 at 18:23 Hi All, I was trying to measure duty cycle and frequency of a pwm signal by using a timer with pwm output to generate pwm signal and another timer in reset mode to measure pwm using one of the example. Th...

nitin29 by Associate II
  • 1028 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.