STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPDIF input capture with STM32F7

Posted on July 28, 2016 at 15:12Hello,I am trying to capture the SPDIF input packets received on STM32F7. I am using a LPCM Stereo input from a DVD player. DMA stream 1 is configured to receive data samples from SPDIF stream. I am receiving a Synchr...

STM32 Example code

Posted on July 27, 2016 at 22:51I keep seeing references online to demo code for the ST chips. Where exactly is it? I have went through through all the Atollic folders, but found nothing. I have went through the CubeMX folders and also found nothing...

achin by Associate II
  • 2603 Views
  • 2 replies
  • 0 kudos

Error in STM32F4 V1.7.1 Std Periph Lib

Posted on July 28, 2016 at 05:58 In the file stm32f4xx.h < br >#define DBGMCU_APB1_FZ_DBG_TIM1_STOP ((uint32_t)0x00000001)< br >#define DBGMCU_APB1_FZ_DBG_TIM8_STOP ((uint32_t)0x00000002)< br >#define DBGMCU_APB1_FZ_DBG_TIM9_STOP ...

X-CUBE-MEMSMIC1 does not compile for NUCLEO-L476RG

Posted on July 28, 2016 at 14:35When I compile the sample firmware for the NUCLEO-L476RG board using the provided project for the Keil IDE, I get the following error:STM32F4xx-MEMSMIC1\STM32L476-MEMSMIC1.axf: Error: L6218E: Undefined symbol APBPresc...

rex by Associate II
  • 758 Views
  • 0 replies
  • 0 kudos

STM32F4 vs STM32L4 on USB audio power consumption?

Posted on July 26, 2016 at 03:17We are currently using the USB audio with the STM32F4, which works well. However, the power consumption of 40mA is something that we want to improve.  Would change to STM32L4 help the situation?  Our use is just using...

andy2 by Associate II
  • 2118 Views
  • 2 replies
  • 0 kudos

Moving on from blinky, how?

Posted on July 19, 2016 at 09:36Hi my name is Etienne, I am new to microcontrollers and I'm still banging my head against the wall.   I would like to run a simple USART printf function to get things going.   To keep it short,  Ive got a Nucleo F103...

rithers by Associate II
  • 4958 Views
  • 11 replies
  • 0 kudos

STM32 CAN Filter

Posted on December 19, 2012 at 14:28The original post was too long to process during our migration. Please click on the attachment to read the original post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.