STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 MP3 USB Streamer

Posted on July 31, 2016 at 00:46STM32F103 Emulating as 1GB USB Disk with 1GB MP3 File to Stream Digital Audio to any USB Porthttp://usbaudiostream.blogspot.com/

Help me speed up my stm32f7

Posted on July 29, 2016 at 19:49Hi everyone,I am making an emulator that is emulating an old c64 computer. For this I am using a custom made hardware. This has a STM32F756 MCU together with 200Mhz SDRAM installed. The real heavy things for this proj...

STM32F303 USB Cube CDC app

Posted on July 28, 2016 at 11:02Some re-edit required:Hi.I have used STM32cubeMX to create a USB CDC application for the NUCLEO-F303RE board. I can connect to the host PC as a CDC, so thats fine.I now want to find in the source code where is the cod...

kvresto by Senior
  • 1424 Views
  • 2 replies
  • 0 kudos

STM32F3 PWM ramp-up/ramp-down

Posted on July 30, 2016 at 10:47Hi everyone,I'm going to work on a motion control project where I want to to generate pulse trains PWM with ramp-up/ramp-down for acceleration. What idea to do this?Thanks! #ramp-up

Setting HSI48 as STM32F072 sysclk

Posted on July 17, 2016 at 16:53I am trying to set HSI48 as my sysclock on STM32F0 Discovery, but by doing this I somehow ended up with an unexpected interrupt and stuck in an infinite loop.I am using True Studio by the way. Not using CubeMX or peri...

Very odd FLOP issue

Posted on July 25, 2016 at 23:00 So I'm currently working on two different STM32F4 boards for two different projects, which share some code between them. These are the F407 disco and F429disco. I recently had to switch to the GCC compiler...

max239955 by Associate II
  • 1969 Views
  • 4 replies
  • 0 kudos

Bug report: stm32f0xx_usart.c v1.5.0

Posted on July 22, 2016 at 12:03In the function:void USART_SetReceiverTimeOut(USART_TypeDef* USARTx, uint32_t USART_ReceiverTimeOut)The code: /* Clear the receiver Time Out value by clearing the RTO[23:0] bits in the RTOR register  */  USARTx->RTOR ...

toni by Associate II
  • 1906 Views
  • 4 replies
  • 0 kudos

vetor table symbol Not found?

Posted on July 27, 2016 at 12:02 I can't debug anymore, I get this message after copying the interrupt table to RAM, even if I comment the Remap() funtion I get this error. Even if I load and try to debug another project I get this error...

jparera by Associate II
  • 4378 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.