STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4DIS-CAM Connector

Posted on August 02, 2016 at 12:10Does the STM32F4DIS-CAM board come with a cable suitable for connecting it to e.g. an STM32F746G-DISCO board? If not, what kind of cable is required for this? Thanks, Harry Wagstaff

harry1 by Associate
  • 1705 Views
  • 3 replies
  • 0 kudos

stm32l432 / openocd

Posted on August 02, 2016 at 15:12I'm starting a project with the stm32l432.   In order to use openocd I had to tweak the sources slightly.   1)  Picked up a version that supports other stm32l4 processors  from  https://github.com/arduino/OpenOCD/ 2...

Displaying icon on TFT ?

Posted on April 14, 2014 at 10:18 Guys, Does anyone of you know on how to display array of bitmap to TFT LCD ? I tried : void LCD_DrawBMPFromFile() { char temp_buffer[100],line[512]; int count,bmpData,bmpAddr; cons...

STM32CubeMX How to Revert to Older Library Version

Posted on August 02, 2016 at 04:52I upgrader to the latest version of the CubeMX library for the F446 and now DCMI doesn't work. Don't have time to chase it down so I'd like to revert to using a previous library version.I tried using the library man...

PWM1 and TIM2 config for dual ADC

Posted on July 27, 2016 at 15:06 Hi, I have a code, kindly provided by clive1, to use two ADC in dual mode on STM32F334, and it works well. I can modify some parameters, but something (the ADC itself, the DMA to fill the memory array, or ...

antoine by Associate II
  • 3086 Views
  • 8 replies
  • 0 kudos

STM32F103VBT6 debugging problem

Posted on August 03, 2016 at 11:45 Hello there, Recently I developed a PCB board containing the STM32F103VBT6 MCU. Recently, I was using STM32F4 devices without any problems. For this device however, I am unable to debug my target using Segg...

Stop ADC in Continuous Mode

Posted on August 03, 2016 at 08:31Hello there,I'm looking for a possibility to quickly stop and restart the ADC from continuous run on a STM32F446.I use the ADC1 and ADC2 in dual combined regular simultaneous  + injected simultaneous mode with DMA s...

GNU ARM Eclipse plug-ins

Posted on March 05, 2015 at 07:46Mayla,Could you be so kind to update your permanent post and add a link GNU ARM Eclipse plug-ins project? (http://gnuarmeclipse.livius.net/blog/)It is highly portable (Windows/OS X/Linux) and also provides a large co...

System boot mode hardware considerations

Posted on August 02, 2016 at 18:25(This is a resend--the original didn't seem to get posted). Is it advisable to pull-up pins participating in the system bootloader interfaces (USART1  & 2 for the F3)?  If floating, is it possible for the bootloader...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.