STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not compiling...

Posted on August 02, 2016 at 18:37What version of HAL/etc do you have?  I'm not having any luck compiling it with my kit (Keil uVision 5, set to use the F030R8 processor and the 1.4.0 stm32f0xx_hal.h)...

Setting Up Variable Speed Timer on STM32F4

Posted on August 01, 2016 at 20:55I am working on a project that would benefit from a timer whose speed could be changed in real time within the program. Right now I have a timer set up with Tim_CMD, but the prescaler for that is set when it is init...

epalaima by Associate II
  • 1499 Views
  • 4 replies
  • 0 kudos

ST Motor Control firmware

Posted on August 02, 2016 at 14:00Hi,   I would like to evaluate ST's motor control libraries. I have the motor control workbench, which looks great. I would now like the software libraries - the actual motor control code, PMSM, not BLDC, so I can l...

tau by Associate II
  • 1095 Views
  • 1 replies
  • 0 kudos

Trace function too slow? (Keil)

Posted on August 02, 2016 at 14:43I use two ADCs, working together on two different signals.These two signals have the same frequency and amplitude. They are shifted, Signal 2 has a phase of 90°.The DMA put the converted values in an array. This arr...

0690X00000605QcQAI.png
antoine by Associate II
  • 1692 Views
  • 2 replies
  • 0 kudos

STM32CubeMX: not all pins are shown

Posted on July 29, 2016 at 17:46I'm using STM32F746ZGT6 device.I select SPI2 and software gives me 27,28,69,73 pins.But there are other pins that can be used for SPI2.73,74,75,76 for instance.How to make software to show other sets of pins?Thanks

load2005 by Associate III
  • 1399 Views
  • 3 replies
  • 0 kudos

STM32F4-DIS, camera 5mp, DCMI interface

Posted on July 19, 2016 at 17:32Hi,I'am starting a new project and I will need to interface the STM32F4-discovery with a camera ( 5mp ),can you suggest me a DCMI camera module with 5mp resolution

Delay with Center Aligned PWM triggering an ADC conversion

Posted on August 01, 2016 at 16:28Hi,I’m using a stm32f103 to generate center aligned PWM on which i have synced a dual regular simultaneous injected mode ADC conversion.I’m using TIM4 as source of the PWM signal and, to launch the ADC acquisition a...

0690X00000603AIQAY.jpg 0690X00000603ANQAY.jpg
davide by Associate II
  • 2228 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.