STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What wireless communication module with libraries (Wifi?)

Posted on August 21, 2016 at 19:38Is there a wireless module or chip with libraries. The possibility of an external antenna is a plus, in case of metal box. I tried NRF24 modules. they have libraries around the net but I could not get them to compil...

LMI2 by Lead
  • 1102 Views
  • 2 replies
  • 0 kudos

software expansion package for STM32Cube

Posted on October 07, 2015 at 14:20Hello,Does anyone know how to install a software expansion  package for STM32Cube. Let's say I downloaded X-CUBE-MEMS1.ZIP. I then went to ''Help/Install New Libraries'' then clicked on ''From Local...'' I selected...

STM32F0 SPI Timeout Error with illegal HAL state

Posted on August 19, 2016 at 12:28 Hello, [I have just written my issue in detail and it has been deleted when I clicked Ok. Thanks, I will write it again though.] We are using the STM32F072CB with the HAL driver in our application a...

janos2 by Associate II
  • 1821 Views
  • 4 replies
  • 0 kudos

Interrupts Don't Fire Up in HAL SPI

Posted on July 31, 2016 at 21:34The original post was too long to process during our migration. Please click on the attachment to read the original post.

nitin29 by Associate II
  • 1310 Views
  • 1 replies
  • 0 kudos

HAL_UART_Receive_IT returns error

Posted on August 04, 2016 at 09:48 Hi, I want to transmit something from PC to uC and I put UART in receive mode. However HAL_UART_Receive_IT keeps returning error, and I don't know why? My code is really simple: int main(void){/* Reset...

STM Virtual Com Port Driver for Windows 10

Posted on June 04, 2016 at 01:21I downloaded the VCP_V1.4.0_Setup.exe and ran it. But it only has Win7 and Win8 directories. Does anyone if either of them will work on 64-bit Windows 10? If neither will work then where can I get the STM VCP driver f...

gaurav2 by Associate II
  • 21577 Views
  • 4 replies
  • 0 kudos

BUG - HAL_SPI_Receive (STM32F0 & CubeF0)

Posted on August 16, 2016 at 14:20 Hi All HAL_SPI_Receive function has a strange problem, a simple workaround can be implemented as a temporal solution but I need reason of the this behaviour. address = 0x138001; // Ext_Flash_W...

0690X00000603C4QAI.jpg 0690X00000603B6QAI.jpg 0690X00000603BkQAI.jpg 0690X00000603B7QAI.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.