STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMCubeMX HAL: User Code includes in generated code

Posted on September 27, 2016 at 15:54I'm using System Workbench for STM32 and working with an STM32F7 with the HAL libraries.I'm working with a VCP and I'm looking at capturing the input buffer in the usbd_cdc_if.c and sending it to a parsing routin...

Proper way to turn off PWM channel

Posted on September 27, 2016 at 13:35Hello there, I am using STM32F4 to drive a 3 phase BLDC motor. With this motor when using block driving (or trapezoidal), one of the 3 outputs should always float. What registers should be set exacly in order to ...

STM32 F2/F4 USB Host issues

Posted on October 16, 2014 at 11:30 .ExternalClass11B1744985E14676887C8F042F0B5239 p {margin-bottom:0.1in;line-height:120%;} Hi,I am writing a host stack and I have noticed various issues with the documentation and the hardware.Issue #1The pdf in...

miro_atc by Associate II
  • 4886 Views
  • 8 replies
  • 1 kudos

STM32F103C6T6A clock configuration

Posted on September 27, 2016 at 17:30I need to configure the system clock to HSE with a 8MHz quartz crystal.At startup the default is HSI. For the STM32L family I used the clock configuration tool provided by ST, but this tool is not available for S...

Jump to user application in the USB_Device/DFU_Standalone Example

Posted on September 27, 2016 at 14:48Hello,I am using STM32Cube_FW_L4_V1.5.1 library and I am trying to test the STM32Cube_FW_L4_V1.5.0\Projects\STM32L476G_EVAL\Applications\USB_Device\DFU_Standalone application. I have STM32L476RG-Nucleo + NUCLEO-C...

dpn by Associate II
  • 2032 Views
  • 3 replies
  • 0 kudos

CAN is getting stuck in initilaztion

Posted on September 27, 2016 at 03:34Hi,I m using STM32F303XC processor.I configured the CAN at 250 kbps baud rate. but it is getting stuck in following while loop. CAN is not able initialize properly.What would be the problem to getting stuck in in...

SS.Sagar by Associate III
  • 1673 Views
  • 4 replies
  • 0 kudos

STM32F407 Dual DAC Independent Trigger Sources

Posted on September 27, 2016 at 08:54Hello,I have a problem for using both DACs of STM32F407 with independent trigger sources. What I did was directing DAC1 for Timer6 and DAC2 for Timer7 but they are still both triggered by one source (Timer6) and ...

yousef by Associate
  • 1432 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.