2016-09-26 11:54 PM
Hello,
I have a problem for using both DACs of STM32F407 with independent trigger sources. What I did was directing DAC1 for Timer6 and DAC2 for Timer7 but they are still both triggered by one source (Timer6) and not independent as described. I set TSEL1 and TSEL2 for the sources accordingly (TIM6_TRGO, TIM7_TRGO). I tested both Timer Interrupts to be invoked as working.DMA is not used in my case.Are there any known issues for this topic?Thanks in advance, Sebastian.2016-09-27 5:12 AM
If you're not using DMA, why are you triggering the DAC's from timers? What is it that you're trying to achieve?
2016-09-27 8:49 AM
Are there any known issues for this topic?
Haven't heard of any, and don't plan to independently verify. If you want someone to review the code for errors/issues, you'll want to post a sufficiently complete example.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.