STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flush USART RDR after receiving

Posted on September 27, 2016 at 17:11Dear all,I am using STM32F4 Discovery board and have some problems with using DMA on USART. The cause may be the unwanted left behind data inside USART RDR.Would you please kindly give me instruction how can I fl...

Problem with debugging & IWDG with STM32F407VGT6

Posted on September 21, 2016 at 15:56Since firmware version 1.13 there is a big issue with debugging. The firmware starts the watchdog during initialization. This result in reset when a breakpoint reaches. Before this version, I could start the IWD...

Osto by Senior
  • 1253 Views
  • 2 replies
  • 0 kudos

STM32F411 Errata

Posted on September 24, 2016 at 16:20Is there a new version of the Errata document? The one the website (Doc ID 027036) is revision 1 and was released on 20-Oct-2014.Why do I ask? The STM32F412 - has an Errata about DMA2 corruption when managing AHB...

STM32 Cube MX bootloaded application

Posted on September 27, 2016 at 09:56Does anyone know if it is possible to get STM32 CubeMX to generate a project that is ''predefined'' to be loaded using a bootloader?Essentially, this would involve being able to specify the program load address a...

Mouse and Keyboard USB HID stm32f042

Posted on September 26, 2016 at 18:14In separate applications I have managed to control the mouse, and the keyboard using the stm32f042. How do I go about combining the two in one application?I would like my stm32 to be treated as both a keyboard an...

STM32F769I - Possible CAN errata

Posted on September 20, 2016 at 20:29 During evaluation of this chip, we found thatthe microcontroller apparently sets the ACK bittoo early when receiving messages from other devices. Bus was 250 KBaud with a sample point of 80% (also tried 75% a...

holeman by Associate II
  • 2409 Views
  • 5 replies
  • 0 kudos

SPI Slave Tx DMA wont stop

Posted on September 26, 2016 at 09:12 In my application STM32F411 is a SPI slave (TI mode) and the master microcontroller transmits data as packets perpetually till an acknowledgement is received from STM After a packet of data is received by ST...

siva by Associate
  • 984 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.