2016-10-05 1:38 AM
I can't install the VCP Driver from the ST site for my stm32f4-Discovery on Windows Embedded. Is there any Solution or special Driver ?
2016-10-05 2:11 AM
Hello,
VCP downloadable at . Then v4.0.0 should be sufficient to connect to the board and provide a VCP interface.Regards2016-10-05 2:46 AM
I get always the message ''A Service Installation Section in this INF is invalid''.
2016-10-05 3:13 AM
Hi,
Make simple search in Google to find several links and video about this error that helps you and guide you to solve this: , .Regards2016-10-05 7:07 AM
Hi,
In the readme file of the ''STM32 Virtual COM Port Driver'' packageSTSW-STM32102, it is mentionned that th SW support only
Windows 98SE, 2000, XP, Vista, Seven, 8.x (x86 & x64 Windows platforms) . -Hannibal-2016-11-03 9:46 AM
The solution for Windows Embedded 7
https://social.msdn.microsoft.com/Forums/en-US/56315793-9a01-4cf4-8991-24cc749c9d9a/missing-usbsersys-windows-7-embedded?forum=quebecmisc2016-11-03 11:10 AM
Amazing! And how should we connect to STM32 USB in Windows Embedded 7?
I think ST believes you should have in-house competence in the OS you have chosen. Whether that extends to writing drivers from the DDK, or modifying installers or .INF, or getting one's own products through WHQL, etc.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.