STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DAC DMA is giving error in stm32f3xx_hal_msp.c

Posted on November 27, 2016 at 01:50 Hello! I am currently using stm32mx cube to create sine wave through the DAC. When I am building the project, I am receiving an error in regards to the stm32f3xx_hal_msp.c which should not require any ...

kl4971tse by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

This forum is useless

Posted on November 23, 2016 at 15:32I wanted to post an answer but couldn't reply even though I am able to login and post. That is the largest problem of the STM32F CPUs.

LMI2 by Lead
  • 1180 Views
  • 5 replies
  • 0 kudos

Why comdef.h need for stm32f070xx ? not working!

Posted on November 22, 2016 at 07:56Dear All,Does the comdef,h file not support in KEIL if we build code for stmf070xx type device?With the reference, http://stackoverflow.com/questions/157101/where-can-i-get-comdef-h. kindly tell me why we need thi...

How to tell if other CAN device is present on bus?

Posted on November 28, 2016 at 04:58I would like to know if there is another device present on the CAN bus.  Is there a way to do this without too much overhead?  I have my STM32F4 setup and communicating on a CAN bus.  Sometimes there is another de...

I2C Questions on STM32F427

Posted on November 25, 2016 at 09:35I have a slave device which is address 0x78 for write and address 0x79 for read.I want to confirm that why the below I2C transaction is difference?I want to reset the slave device and the mapping register informat...

0690X00000605SxQAI.png 0690X00000605SUQAY.png
pohua by Associate II
  • 1276 Views
  • 2 replies
  • 0 kudos

ST-Link V2 dongle broken?

Posted on November 26, 2016 at 11:20Purchased from Mouser 1.5 years ago but not used until now. I am getting ''Can not connect to target!'' error message in ST-Link Utility whether I try my Mini-M4 for STM32 (415RG, JTAG/SWD) or my Discovery board (...

parsec by Associate III
  • 2202 Views
  • 4 replies
  • 0 kudos

ST-Linkv2 Pod: Connection in ''Low Power Mode''

Posted on November 27, 2016 at 00:48Hi, Sorry if this question may have been answered, I was unable to find anything in the forum on this. Using an STM32F405/64pin device. Boot 0 is tied to GND through a 470R resistor. Since I'm using flash boot, I ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.