2016-12-16 5:27 AM - edited 2024-12-09 10:16 AM
2016-12-16 11:12 AM
Hi
sylvain
,You should checkif the new LSE source (crystal/oscillator) is correct - > check the table.7 of application note
Second, the used project generated from the CubeMx is for the STM32F3-Disco hardware ; the workspace will include many HW dependencies you would check -> I advise you to regenerate another project using the .ioc file with selection you new board or simply the device.
-Walid F-
2016-12-17 8:40 AM - edited 2024-12-09 10:15 AM
-
2016-12-20 5:59 AM
The STM32 devices don't function properly with the 9pF and 12pF 32.768 KHz crystals that are quite common. You want one of the 6-7pF variety, and review the performance of the circuit with the components as built. The most common failures are taking a long time to start, or not starting, and frequency being off or unstable.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.