STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 ADC/DMA in DUALMODE

Posted on December 30, 2016 at 02:05The original post was too long to process during our migration. Please click on the attachment to read the original post.

Resolved! PWM for PB0 not firing, stm32f051

Posted on January 04, 2017 at 20:25I am not sure why the following code is not working. I have used it before for a different pin, but I believe my modifications would allow this to work? I am running the code on the stm32f051 discovery board using ...

Display a simple string with STM32F429I DISCO-BOARD

Posted on September 04, 2015 at 23:22Hello, I recovered some examples to display some string on my DISCO-BOARD, but the example that I found are all build with Drivers/BSP/STM32F429I_DISCO which use as source and header files ==> stm32f429i_discover...

When does ADC/DMA actually stop?

Posted on January 05, 2017 at 15:20In my project (F415RG) I'm running timer paced single channel ADC sampling with DMA transfers and Analog Watchdog coupled to the same ADC channel. When an out of window voltage occur I need to momentarily stop the ...

parsec by Associate III
  • 738 Views
  • 0 replies
  • 0 kudos

Is ADC sampling clock equal to system clock ?

Posted on December 30, 2016 at 13:40hello dear forum,I am trying to take 500 samples from STM32F103RC ADC with DMAI wanna know if the ADC sampling clock equal to ADC clock or system clock for example ;If I choose ADC clock = P2clock / 8 = 9 MHz and ...

GPIO interrupt problem

Posted on January 04, 2017 at 19:52Hi everybody.I have to implement a Wiegand reader on a STM32 demo board.Using CubeMX I have defined 2 gpios as GPIO_EXTI and now the HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) is triggered.The problem is that the ca...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.