2017-01-03 5:12 PM
Hey all,
Been poring over the STM32Cube HAL documentation for the better part of the day, scouring both the DAC and DMA portions for STM32F3 (device I'm using specifically is the STM32F373), and I can't find any way to configure the DAC and DMA for dual output mode. It seems between CubeMX code generation and the docs there's no explicit way to set up DMA to transfer 2 channels of data via synchronized dual channels. Does this 'automagically' happen for DMA, or will I need to manually configure the channels outside of Cube configuration?
My goal is to have a single routine generate samples for both outputs of DAC1, then store them in a buffer to be shuffled off to the DAC via DMA. I've done this with the STM32F1 and the Standard Peripheral Library, but don't find an equivalency in STM32Cube. Any suggestions?
Thanks!
2017-01-05 6:41 PM
Alright, after digging in for a couple days of code analysis, the short answer is no, STM32Cube HAL will not directly support DAC dual mode with DMA. What I've done for now is fairly hackish, but it gets the job done right now. If anyone wants to clean this mess up, I'm all ears.
To get Dual DMA working in STM32Cube, I cloned the HAL_DAC_Start_DMA function and modified it for use. I created a #define of DAC_CHANNEL_12R which tells the function to 'turn on' dual mode. The specific changes were extremely simple: Add a third case for using both channels synchronously, pointing the DMA transfer to the correct DHR*D register instead of DHR*[12] register, and then turning on both DAC outputs. Currently it only supports dual mode via Channel 1 DMA, it could easily be expanded for Channel 2 DMA operation but I have no need for it. Here are the snips of code from my application for use/review:
#define DAC_CHANNEL_12D ((uint32_t)0x00000011)
HAL_StatusTypeDef HAL_DAC_Start_DualDMA(DAC_HandleTypeDef* hdac, uint32_t Channel, uint32_t* pData, uint32_t Length, uint32_t Alignment){ uint32_t tmpreg = 0; /* Check the parameters */ assert_param(IS_DAC_CHANNEL_INSTANCE(hdac->Instance, Channel)); assert_param(IS_DAC_ALIGN(Alignment)); /* Process locked */ __HAL_LOCK(hdac); /* Change DAC state */ hdac->State = HAL_DAC_STATE_BUSY; if(Channel == DAC_CHANNEL_1) { /* Set the DMA transfer complete callback for channel1 */ hdac->DMA_Handle1->XferCpltCallback = DAC_DMAConvCpltCh1; /* Set the DMA half transfer complete callback for channel1 */ hdac->DMA_Handle1->XferHalfCpltCallback = DAC_DMAHalfConvCpltCh1; /* Set the DMA error callback for channel1 */ hdac->DMA_Handle1->XferErrorCallback = DAC_DMAErrorCh1; /* Enable the selected DAC channel1 DMA request */ SET_BIT(hdac->Instance->CR, DAC_CR_DMAEN1); /* Case of use of channel 1 */ switch(Alignment) { case DAC_ALIGN_12B_R: /* Get DHR12R1 address */ tmpreg = (uint32_t)&hdac->Instance->DHR12R1; break; case DAC_ALIGN_12B_L: /* Get DHR12L1 address */ tmpreg = (uint32_t)&hdac->Instance->DHR12L1; break; case DAC_ALIGN_8B_R: /* Get DHR8R1 address */ tmpreg = (uint32_t)&hdac->Instance->DHR8R1; break; default: break; } } else if(Channel == DAC_CHANNEL_2) { /* Set the DMA transfer complete callback for channel2 */ hdac->DMA_Handle2->XferCpltCallback = DAC_DMAConvCpltCh2; /* Set the DMA half transfer complete callback for channel2 */ hdac->DMA_Handle2->XferHalfCpltCallback = DAC_DMAHalfConvCpltCh2; /* Set the DMA error callback for channel2 */ hdac->DMA_Handle2->XferErrorCallback = DAC_DMAErrorCh2; /* Enable the selected DAC channel2 DMA request */ SET_BIT(hdac->Instance->CR, DAC_CR_DMAEN2); /* Case of use of channel 2 */ switch(Alignment) { case DAC_ALIGN_12B_R: /* Get DHR12R2 address */ tmpreg = (uint32_t)&hdac->Instance->DHR12R2; break; case DAC_ALIGN_12B_L: /* Get DHR12L2 address */ tmpreg = (uint32_t)&hdac->Instance->DHR12L2; break; case DAC_ALIGN_8B_R: /* Get DHR8R2 address */ tmpreg = (uint32_t)&hdac->Instance->DHR8R2; break; default: break; } } else { /* Dual-channel mode - added by JG @ Det3 */ /* Set the DMA transfer complete callback for channel1 */ hdac->DMA_Handle1->XferCpltCallback = DAC_DMAConvCpltCh1; /* Set the DMA half transfer complete callback for channel1 */ hdac->DMA_Handle1->XferHalfCpltCallback = DAC_DMAHalfConvCpltCh1; /* Set the DMA error callback for channel1 */ hdac->DMA_Handle1->XferErrorCallback = DAC_DMAErrorCh1; /* Enable the selected DAC channel1 DMA request */ SET_BIT(hdac->Instance->CR, DAC_CR_DMAEN1); /* Case of use of channel 1+2 - dual mode */ switch(Alignment) { case DAC_ALIGN_12B_R: /* Get DHR12RD address */ tmpreg = (uint32_t)&hdac->Instance->DHR12RD; break; case DAC_ALIGN_12B_L: /* Get DHR12LD address */ tmpreg = (uint32_t)&hdac->Instance->DHR12LD; break; case DAC_ALIGN_8B_R: /* Get DHR8RD address */ tmpreg = (uint32_t)&hdac->Instance->DHR8RD; break; default: break; } } /* Enable the DMA Channel */ /* Reversed for dual-channel operation by JG @ Det3 */ if(Channel == DAC_CHANNEL_2) { /* Enable the DAC DMA underrun interrupt */ __HAL_DAC_ENABLE_IT(hdac, DAC_IT_DMAUDR2); /* Enable the DMA Channel */ HAL_DMA_Start_IT(hdac->DMA_Handle2, (uint32_t)pData, tmpreg, Length); } else { /* Enable the DAC DMA underrun interrupt */ __HAL_DAC_ENABLE_IT(hdac, DAC_IT_DMAUDR1); /* Enable the DMA Channel */ HAL_DMA_Start_IT(hdac->DMA_Handle1, (uint32_t)pData, tmpreg, Length); } /* Process Unlocked */ __HAL_UNLOCK(hdac); /* Enable the Peripheral */ if(Channel == DAC_CHANNEL_12D) { __HAL_DAC_ENABLE(hdac, DAC_CHANNEL_1); __HAL_DAC_ENABLE(hdac, DAC_CHANNEL_2); } else { __HAL_DAC_ENABLE(hdac, Channel); } /* Return function status */ return HAL_OK;}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.