2016-12-30 4:40 AM
hello dear forum,
I am trying to take 500 samples from STM32F103RC ADC with DMA
I wanna know if the ADC sampling clock equal to ADC clock or
system clock
for example ;
If I choose ADC clock = P2clock / 8 = 9 MHz
and I choose sampling time 239.5 clock
does this mean that 500 samples last ( 239 * 500 ) / 9000000 = 13 milisecond ?
thank you
#stm32f103-adc-clock2016-12-30 5:48 AM
There is also the conversion time, which is dependent on the number of bits. The computation is in the reference manual as I recall.
For a specific 'sample rate', in the I want 1 KSps sense, you'd do better configuring a TIM based trigger rather than play games with the sample+conversion numbers and the limited subset of choices that provides.
2016-12-30 9:39 AM
hello thank you Clive ,
I have the following problem;
I want measure the peaks in the signal below picture
this is current signal from current transformer output of a power electronics device
the signal is line synchronized as you expect ( but I already have PCB printed and I havenot made an HW interrupt for line zero crossing so I cant synchronize my ADC with the signal )
one idea which came into my mind
is measuring more than 10 milisecond and finding the peak ( or 10 samples from both sides of peak and averaging the result ) with software
my first question ; if I select ADC clock 9 MHz and sampling time 240 clocks and taking 500 samples with DMA - do the 500 samples last about 13 milisecond ?
second ; what other suggestion do you make to me ? how can I measure peak current from above signal picture with only having ADC input in my hand?
2016-12-30 10:11 AM
The conversion is an additional 12.5 cycles, so 239.5 + 12.5 = 252 cycles
500 samples with a 9 MHz ADC clock would be 14 ms
You can benchmark/qualify these things yourself by toggling a pin in a 500 sample DMA TC interrupt, or timestamp with DWT_CYCCNT
You could shoot to have a 10ms sample buffer, or one split it two halves, that you could process at 100Hz. ie find the peak, should remain in roughly the same spot in the buffer. If you used a TIM trigger, you could advance or r.etard slightly the sample rate to keep it centred, or follow it
2016-12-30 11:37 PM
How about filling up a SRAM buffer of ADC sample by DMA in circular mode (no interrupt) and activate the analog watchdog to capture by interrupt the DMA sampling area for analysis of peak value etc... ?
2017-01-05 6:15 AM
hello Clive ,
please I have one more question
if I scan 2 different analog inputs each with 239 cycles sampling time ,
does the sampling times overlap ?
or , do every single channel wait 239 cycles sampling before ADC conversion ?
i.e. for 2 channels conversion 2 x 239 = 478 cycles sampling time in total ?
thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.