2017-01-11 12:22 PM
Hi,
Here is my program
#include <stdio.h>
#include <string.h>#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'#include 'stm32f10x_usart.h'#include 'stm32f10x_spi.h'#define SPI_FLASH SPI3#define SPI_CLK RCC_APB1Periph_SPI3#define SPI_GPIO GPIOC#define SPI_GPIO_CLK RCC_APB2Periph_GPIOC#define SPI_PIN_SCK GPIO_Pin_10#define SPI_PIN_MISO GPIO_Pin_11#define SPI_PIN_MOSI GPIO_Pin_12void SPI3_IRQHandler(void){ USART_SendData(USART1,SPI_I2S_GetITStatus(SPI3, SPI_I2S_IT_TXE)+48) ; SPI_I2S_ClearFlag(SPI3,SPI_I2S_IT_TXE); }void SPIConfig(void){SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable SPI and GPIO clocks */ RCC_APB2PeriphClockCmd( SPI_GPIO_CLK , ENABLE);RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3,ENABLE); GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE); /* Configure SPI pins: SCK, MISO and MOSI */ GPIO_InitStructure.GPIO_Pin = SPI_PIN_SCK | SPI_PIN_MISO | SPI_PIN_MOSI; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(SPI_GPIO, &GPIO_InitStructure); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI3, &SPI_InitStructure);SPI_I2S_ITConfig(SPI3,SPI_I2S_IT_TXE,ENABLE);SPI_I2S_ITConfig(SPI3,SPI_I2S_IT_RXNE,ENABLE); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); NVIC_InitStructure.NVIC_IRQChannel = SPI3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable the SPI */ SPI_Cmd(SPI3, ENABLE);} void delay(){ int i,j; for(i=0;i<10000;i++) for(j=0;j<250;j++);}int main(){ unsgined char p[3] SPIConfig(); while(1){ delay();delay(); USART_SendData(USART1,'A') ; } } }But it prints '1' char continuously and it doesn't arrive at USART_SendData(USART1,'A') ; line to send 'A' char to terminal while I didn't send & receive anything.what is my mistake?
Solved! Go to Solution.
2017-01-11 1:35 PM
>>
what is my mistake?
Unless you actually send some data TXE is going to continue to assert until you disable it. Clearing the IT flag isn't sufficient.
You'd also do well to qualify the source of the interrupt in the IRQ Handler
2017-01-11 1:35 PM
>>
what is my mistake?
Unless you actually send some data TXE is going to continue to assert until you disable it. Clearing the IT flag isn't sufficient.
You'd also do well to qualify the source of the interrupt in the IRQ Handler
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.