STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 how to support two network interface

Posted on January 17, 2017 at 04:08Hi:I use STM32F4 series and it works OK for one network PHY (using LwIP). As I know the F4 MAC interface can read/write  more than one PHY's. However only one set of MII/RMII interface pins and MAC hardware, imply ...

STM32CubeMX Mac Problem During Download

Posted on September 09, 2016 at 18:46I've tried installing STM32CubeMX on two different Macs. In both cases when I try to download firmware kits, I get an error ''These Files have a problem during Download''. I've also tried downloading the zip file...

phroggie by Associate II
  • 3782 Views
  • 10 replies
  • 0 kudos

Resolved! STM32F413 SRAM2 through I-Code/D-Code bus.

Posted on January 17, 2017 at 14:59Hi, I want to use the STM32F413 SRAM2 to run interrupt control loop routines, as I do for CCM-SRAM of the STM32F303. So I need to configure the SRAM2 to be acessed through the I-Code/D-Code bus (address 0x10000000)...

Asantos by Senior
  • 1263 Views
  • 2 replies
  • 0 kudos

fatfs disk error

Posted on January 11, 2017 at 14:59Hi,I am using fatfs sdio with my stm32f429 mcu , i can, open read, write files correctly. When i plug out the sd card from my board at runtime, the f_open, f_write and f_read functions do not work and so i can not ...

er3481 by Senior
  • 3225 Views
  • 6 replies
  • 0 kudos

stm32f7 NOR flash ,

Posted on January 16, 2017 at 16:43A real simple questoin here, I'm  a hardware guy...sorry.Looking at the stm32F7 data sheets, and using the fmc in NOR flash mode. From the software perspective, would you have a lump of code that does the sequence ...

Proper way to use Cube_FW_ templates?

Posted on January 17, 2017 at 05:21How am I supposed to use these? I'm using SW32STM Workbench and can build projects from STM32CubeMX-generated code. I can build and run code from the Cube_FW_Fx examples.But when I try to copy the files from the Te...

Modify of HAL_PWR_EnterSLEEPMode() function

Posted on January 17, 2017 at 13:39I�m working on a time critical application with OpenSTM32 System Workbench for STM32 . I�d like to reduce the call time of HAL_PWR_EnterSLEEPMode(uint32_t Regulator, uint8_t SLEEPEntry). The code : void Sleep( uint...

eMMC in 8 bits Wide bus mode

Posted on January 04, 2017 at 15:35Hello,I'm using a STM32L4 and CubeMx to generate eMMC code, either the 8 bits wide bus mode configuration isn't supported and should be configured manually.I was able, with few code modification, to use the SD auto...

Spi dma: can't change spi prescale

Posted on January 16, 2017 at 16:10Hi,I'm trying to get spi driver working for ad-converter. Adc spi is supporting ~20mhz spi clock. Now my project APB2(Using spi1) clock is 84 Mhz and spi prescale is now 2( Spi clock is 42Mhz) and code is running f...

teijo by Associate II
  • 1783 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.