2016-09-09 9:46 AM
I've tried installing STM32CubeMX on two different Macs. In both cases when I try to download firmware kits, I get an error ''These Files have a problem during Download''. I've also tried downloading the zip files and installing ''from local'' which also fails.
I know it's not an access problem since I tried installing STM32CubeMX on a virtual session of Windows XP on one of the computers and downloading the firmware kit and it worked without any problems.Is there something I'm missing?Peace2016-09-16 6:25 AM
Hi phroggie,
Is this problem solved ? Regards2016-09-20 4:50 AM
Dear user,
Can you please send us the STM32CubeMX.log file you find under your user directory in the .stm32cubemx folder.
Thanks
2016-10-02 7:36 PM
Sorry for the delay.
________________ Attachments : STM32CubeMX.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzQP&d=%2Fa%2F0X0000000bLj%2FZEHZXmks4G4DZKXoH_BAK3ARfpyu_JpfoeolqOyaOg0&asPdf=false2016-10-03 7:03 PM
I'm not sure the attachment was included correctly so I'm trying again.
________________ Attachments : STM32CubeMX.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htpj&d=%2Fa%2F0X0000000aXU%2FMwyAAqw._Z6NdGqha1i9uNHUJQgnJ3gajNP4kzBfi24&asPdf=false2016-10-03 7:10 PM
I've tried to upload the file twice in Safari but when I try to view it, I get a 404 error. I'm now trying with Firefox.
________________ Attachments : STM32CubeMX.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htit&d=%2Fa%2F0X0000000aWA%2FGwTNDIL5mxQ7QSmOQsBx0JjjgOFXO7WJoMnl0Zz06fo&asPdf=false2016-10-07 9:44 AM
2017-01-16 1:41 AM
Hello
Lemberg.Roger
,I tried to reproduce your issue and it was easy to reproduce it.
I deleted the firmware F7 and tried to download it (automatically) in help/Install New Librairies.
2 times the download failed with the following error (There files have problem during download ... (MD5 file checksum is not good).
I can't see STM32Cube_FW_F7_v1.5.1in the STM32Cube/repository so for me, it is a problem of download and not on MD5sum (as MD5sum is the same for Windows, mac and linux and I don't have any issue when downloading on Windows). Moreover, if the file is not correctly downloaded, for sure, MD5sum will be wrong.
I tried a 3rd time to download automatically F7_V1.5.1 and it works. So for me, it is linked to a network issue.
How many times did you try to download the fw?
Could you please try again and ensure that the network is ok?
BR. Eric
2017-01-16 5:53 PM
Since I had no problem getting the files through a virtual machine, I really don't think the network was the problem.
I did actually find a solution: I poked around in the app's package and I found an uninstaller executable. After running it and reinstalling from scratch it now works on both Sierra and El Capitan.
2017-01-17 1:44 AM
Thanks for your information phroggie.
For my information, on which cubeMX release are you? (4.16.1, isn't it?)
BR. Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.