2017-01-16 8:21 PM
How am I supposed to use these? I'm using SW32STM Workbench and can build projects from STM32CubeMX-generated code. I can build and run code from the Cube_FW_Fx examples.
But when I try to copy the files from the Templates into a new directory then import it, it takes some hand-waving to add all the includes, and even then, it complains of a missing target.
Building file: /Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s
Invoking: MCU GCC Assembler/Users/john/src/stm32/stm32f7xx/templt/SW4STM32/STM32F769I_DISCOVERY_AXIM-FLASH/Debugarm-none-eabi-as -mcpu=cortex-m7 -mthumb -mfloat-abi=hard -mfpu=fpv5-sp-d16 -g -o 'Example/SW4STM32/startup_stm32f769xx.o' '/Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s'Finished building: /Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s make: *** No rule to make target `/Users/john/src/Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.c', needed by `Drivers/STM32F7xx_HAL_Driver/stm32f7xx_hal.o'. Stop.21:25:23 Build Finished (took 2s.702ms)
I'm doing something improperly and I am not sure what. Goal is a template that includes BSP and syscalls.c Please advise.
2017-01-17 2:11 AM
Hello
doe.john.016
,You can refer to this thread it will hep you on
https://community.st.com/0D50X00009XkeN3SAJ
.In the STM32CubeF7 firmware package, you may find pre-configured projects for the SW4STM32IDE as well as a template project.
You may use them as a start pointto have more idea on how configuration/implementation is done.
Regards
Imen
2017-01-17 4:42 AM
The templates only work when I use them in place with their original name. How do I copy the template into a different filename and still get everything to resolve?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.