STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI 8bit data length

Posted on February 28, 2017 at 16:56Hi, I'm setting up SPI comms with a slave device. (ADXL350 accelerometer) This is on an STM32F767ZIT6. I should point out I put this on a nucleo -'F746 board but it's all working fine so far at 200MHz with other p...

0690X00000603hHQAQ.jpg
tau by Associate II
  • 7832 Views
  • 11 replies
  • 0 kudos

My Stm32L0 working without JP6 ON

Posted on March 01, 2017 at 21:36Hi everyone, i'm currently working with an stm32L053R8 and here's my problem:My board works without the jumper JP6 on. I don't get why.By 'it works' I mean I'm able to connect it to STM Studio and read RTC datas with...

Resolved! ST32F302RC USART with parity not working

Posted on March 02, 2017 at 08:49Hello,I am working on STM32F302RC. I want to use the USART1 with parity enabled both odd/even which is configurable through command.I am using USART1 withbaudrate 115200,data length8 bit ,  parity none with this conf...

ra.pamod by Associate III
  • 5117 Views
  • 14 replies
  • 1 kudos

STM32F415xx flash self write issue

Posted on March 01, 2017 at 16:55I'm developing a firmware for a custom board based on a STM32F415xx microcontroller.The application must read a file from the on-board SD card, parse it and save some data into the microcontroller flash.This is worki...

HAL flash size

Posted on March 01, 2017 at 15:32Hi, can you tell me if it is normal that the stm32 hal use a lot of flash size. For exemple, just to setup the main clock, 3ko is used (3ko is the difference without the setup and with the setup). And when I use a lo...

I2S Interrupt in STM32F407

Posted on March 02, 2017 at 14:17Hi.I would like to use I2S interrupt, So I wrote following code, But none of the call back fanction not excuted!could you please guide me where is my problem ?note: I can get data in a pooling way with HAL_I2SEx_Tran...

nima2 by Associate II
  • 784 Views
  • 0 replies
  • 0 kudos

low level header - download

Posted on February 26, 2017 at 17:15I recently downloaded CubeMX for the F7 again, to check for the LL headers.I'm pleased to find them complete now, at least at first glance. Gonna test it in the next time.But to my suggestion. The whole packet was...

AvaTar by Lead
  • 1693 Views
  • 2 replies
  • 0 kudos

USB mass storage and sd card

Posted on March 02, 2017 at 10:01hello all,i am using stm32f407 discovery and with this i want to share sd card's data with PC using usb mass storage functionality.so for that i have implemented code.i have interfaced sd card in 1-bit mode.and usb i...

Resolved! STM32L031 program does not run.

Posted on February 28, 2017 at 16:221:I have developed a small program for the STM32L031 Nucleo-32 using the example UART_TwoBoards_ComIT. The program run on the STM32L031 Nucleo-32 develop-board. When I load* the program to our own HW it does not s...

We need a large sum of STM32W108CBU64TR.

Posted on February 21, 2017 at 08:42Hi, members.I'm a chief engineer in charge of developping information display with touch faunction.And my team are developping fat stylus pen that can communicate with touch panel.Actually though under mas product...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.