2017-04-21 1:17 AM
Hi,
I am using a IDB05A1 board together with a L073RZ, is it normal that the IDB05A1 is working when i remove the J1 jumper?
I don't get why since there's no connection between 3v3 and VDDThanks in advance
Raphael2017-04-21 2:38 AM
The IDB05A1 is a Bluetooth Low Energy expansion board based on SPBTLE-RF module for STM32 Nucleo.
The L073RZ is an STM32 Nucleo-64 development board with STM32L073RZ MCU, supports Arduino and ST morpho connectivity.
Looking at the schematic for the IDB05A1, J1 is the jumper linking VDD supply for the Bluetooth Low Energy expansion board with the +3V3 supply. However, there are also connections to the microcontroller's PA0 (IRQ), PA7(MOSI), PA6(MISO) and PB3(CLK).
It's likely that the Bluetooth Low Energy expansion board is being powered by parasitically drawing power from PA0, PA7, PA6 and PB3 when they are logic 1 (high). If you set all those pins to Hi-Z or logic 0 (low), the Bluetooth Low Energy expansion board will probably no longer be powered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.