STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

System Workbench - How to copy projects ?

Posted on April 20, 2017 at 17:21Hi,I tried some example ( e.g. example GPIO_EXTI ) from STM32Cube_FW_F4_V1.15.0 on my board STM32F407-Disc.I used System Workbench for STM32 ver. 1.14.  It`s work well if it is in the original directory.But I tried t...

Peko by Associate III
  • 1725 Views
  • 4 replies
  • 0 kudos

STM32F746G-DISCO

Posted on April 20, 2017 at 12:22Can someone please share the physical height of the STM32F746G Discovery board?  Length and width are in the manual, but height is very difficult to find.  Thanks

Suggest which 32bit MCU to use

Posted on April 24, 2017 at 09:50Hello, STM  Community everyone I would like to choose like that ( 2M CMOS Camera ISP Interface + 65K Color LCD or TFT + SRAM ) I looked ST,confused. Please suggest which chip to use (include Camera interface + LCD In...

MICROCODE

Posted on April 24, 2017 at 07:42Hello All,Where do microcode (which is responsible for stacking etc.) gets saved in STM32 if there is no memory inside the processor core?#microcode

STM32F1 and ILI9341

Posted on December 26, 2015 at 20:50Hello,I'm quite new to the ARM development and hope that you can help me.I have a ILI9341 LCD without touch and wanted to display something :)I got the library for an STM32F4 from this site and tried to rewrite it...

kalinic3 by Associate II
  • 2736 Views
  • 7 replies
  • 0 kudos

Do I need a 1.5K pullup on USB D+ line?

Posted on April 22, 2017 at 08:12Do i need a pullup 1.5K resistor on D+ for USB Full Speed when the USB is configured as a Device (peripheral)? I recently build a custom circuit board without the 1.5K pullup and the PC didn't detect it?  unfortunate...

cleonb322 by Associate III
  • 1811 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.