STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

udp packet sender

Posted on May 01, 2017 at 15:08I've implemented on my board the UDP packet server as a task for a board which has to support ethernet, but nothing is defined for the interface.  So far so good.  I send UDP packets to it and it receives and echoes th...

SPI questions

Posted on November 27, 2016 at 23:40I'm using F3 and L4 processors and have a few spi questions1)  In half-duplex mode, how do you receive a single byte with a master ?  two bytes ?  It appears from reading that in this case, the SPI clock runs as l...

USB get slowly by time

Posted on April 29, 2017 at 10:54Hello, I'm using stm32f407vgt6 and I'm sending data from computer(host) to the MCU(device) through USB in FS mode using CDC library, The total data size is 8MByte and I'm sending it 4KByte by 4KByte (2048 times). Wha...

UART problem betwen stm32f407 and fpga

Posted on April 30, 2017 at 10:03Hello,i have a design where a fpga sends a packet of 10bytes at a baud of 57970 to USART2 of the stm32f407VE device.The idea was to use USART2  where RX pin is receiving data from the fpga,  and the TX pin sends the ...

0690X00000606p7QAA.png
Bogdan by Senior
  • 1613 Views
  • 5 replies
  • 0 kudos

STM32F7 CAN Transmit IT Flags

Posted on April 29, 2017 at 22:20Hello guys,The problem appears on CAN2 (don't know yet if it appears on CAN1 or CAN3).I'm using HAL_CAN_Transmit_IT() to send data.In the CAN2_TX_IRQHandler() I call HAL_CAN_IRQHandler().Action:1. Send 1 CAN frame on...

sony_nix by Associate
  • 738 Views
  • 0 replies
  • 0 kudos

DFSDM Analog Watchdog

Posted on April 29, 2017 at 20:20Hi,I'm looking for an example of DFSDM analog watchdog.My MCU is stm32L476RG and my signal source is a mems microphone.could anybody help me ?thanks

DCMI interface on the Open407v-D

Posted on April 29, 2017 at 03:27Hello ,i'm working with the Open407V-D and i'm having problems with the DCMI interface, is there any jumpers to set in order to chose the PIN that i want to work with ? because when i use cable it work but when i put...

sak hos by Associate III
  • 1550 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.