STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC and DMA issues

Posted on January 20, 2017 at 14:55Hi all,I’m using stm32cube mx to set up a project for my STM32L4 discovery board. Please note that I’ve removed a component and have patched pins PC0, PC1 and PC2 to analog voltages for sampling. I’m using MC...

capture image with STM32F4 to OV9655

Posted on May 06, 2017 at 09:17I want to capture image with camera like OV9655 I have looked for some of tutorial however one of these use OV9655 with stm32f407 and in this tutorial camera show enviroment. can anybody help me in that issue. it is my...

25 microSecond (not milli) Interrupt Advice

Posted on September 18, 2015 at 10:43Hi,I would be grateful for some advice on Sampling logic-level signal with a timer.I haven't done embedded programming in a very long time and so have little experience with the current STM32 offering - and at th...

estersci2 by Associate III
  • 3603 Views
  • 10 replies
  • 0 kudos

issue with SDIO on STM32F746

Posted on May 03, 2017 at 22:15Hi everybody,i'm having issue with reading SD card on STM32F746,i need to read file with size 1.5GB from SD card using SDIO with FatFS library,i used CubeMX for clock calculations :external HSE crystal 12MHzPLL: M: /6,...

Resolved! reading SD card on STM32F7

Posted on May 04, 2017 at 15:22Hi there, is there anybody with STM32F7XX and is able to read bigger file (larger than 30MBytes) from SD card until the end ? without DMA ?i'm asking because i tried more types of cards, and i tried to setup clk div fo...

What is the most reliable way for clocking multiple devices

Posted on May 05, 2017 at 20:15I have a SMT32F7 for control one STM32F4 for comms (ETH MII) and the ETH PHY and I was thinking either one of these (Inclining for number 3):But I'm not an expert and would like to know what is the most reliable of the...

0690X00000606x8QAA.png
mazielvc by Associate II
  • 2789 Views
  • 6 replies
  • 0 kudos

E-Paper stm32l0538 Disco

Posted on May 05, 2017 at 14:13Good Morning, I am trying to create a project that le a sensor and shows the information in the e-paper however there are errors in the initialization of the E-paper. Can you help me by informing which libraries I need...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.