2016-09-14 4:01 PM
Hi,
the topic probably explains it all. When creating a new project with CubeMX, there's usually a long list of TODOs showing up under tasks (using Atollic) which makes it rather difficult to set up my own tasks. Example in csmis_armcc_V6.h: /* ToDo: ARMCC_V6: check if __builtin_arm_rbit is supported */ Would it be asked too much to tidy up any leftover //TODO comments from any generated source files before release? Thanks!Solved! Go to Solution.
2017-05-05 1:53 AM
Hi
Roehrig.Valentin
,On CubeMX4.1, I can see only 2 TODO tasks.
I think it answers to your request and I can only advise you to upgrade your CubeMX with the latest release to solve your issue.
BR. Eric.
2016-09-15 4:56 AM
Dear User,
Can you please indicate which version of STM32CubeMX and which product you are dealing with?
Thank you.
2016-09-18 4:03 PM
Hi,
sure: CubeMX v4.16.1, CubeF0 Firmware package v1.6.0 Steps to reproduce: 1. create empty DisocveryF0 Board project for TrueStudio 2. Import project into TrueStudio 3. Click ''Tasks'' in TrueStudio 4. Observe ~20 Tasks saying: TODO ARMCC_V6: check if __builtin_arm_rbit is supp .... cmsis_armcc_V6.h TODO ARMCC_V6: check if .... cmsis_armcc_V6.h TODO ARMCC_V6: check if .... cmsis_armcc_V6.h TODO ARMCC_V6: check if .... cmsis_armcc_V6.h XXX Register index ... stm32f0xx_hal_rcc.h Thanks!2017-05-05 1:53 AM
Hi
Roehrig.Valentin
,On CubeMX4.1, I can see only 2 TODO tasks.
I think it answers to your request and I can only advise you to upgrade your CubeMX with the latest release to solve your issue.
BR. Eric.
2017-05-06 12:25 AM
Hi Eric,
thanks that's good news. Yes, the original request is now quite old so I'm happy to hear things have evolved.
Keep up the good work!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.