STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Program STM32F103C8T6 with Eclipse on a Windows 10 machine

Posted on April 29, 2017 at 04:09OK, I am sold on STM32 big time. The devices I am using are on a development board, but it's the STM32F103C8T6 at the core. It is the same device used to program using STLINK V2 from a discovery board.When I can prog...

BOOTLOADER- How to jump....

Posted on May 09, 2017 at 09:12Dear Community,I want to implement a boot loader routine located in the first flash sector (0x8000000) of a stm32F407 device. After power up the bootloader decides whether the program pointer can jump to the main app l...

jogerh by Associate II
  • 3499 Views
  • 5 replies
  • 0 kudos

How to start with asembler on Cortex M4

Posted on May 12, 2017 at 08:48Hi,I'm new at STM32. (I own DISCOVERY board STM32F411E-Disco) I have written few programs using Cube and HAL but now I need to use assembler.Can you share any sources where should I start to learn using assembler? Any ...

STM32 CubeMX UART

Posted on May 11, 2017 at 15:27Hello St Community,I'm working on STM32F103 RB microcontroller, I've download STM32CubeMX and STM32CubeF1 .I want to show a message on my computer, thanks to a terminal, which I code on my STM32.I know that an example ...

0690X00000606yVQAQ.png

STM32L052T8 USB Support

Posted on May 08, 2017 at 16:55This package for this micro is a 36 pin WLCSP. The datasheet suggests on pg12 that it supports USB but not VDD_USB, unlike others in this range. Does this mean that the USB line voltage comes from normal VDD? 

how to use only one microphone on STM32F469 Dicovery?

Posted on May 12, 2017 at 14:41I am working on sound aquisation with STM32F469 mems microphone, I know that if i want to use one microphone of the three mems microphone , I only have to pick out th JP5. is it true? But when i did that i lose control...

code protection stm32l151cct6

Posted on May 12, 2017 at 13:22I'm using a stm32l151cct6 MCU and I want to protect a sector of the flash memory using Option Bytes in ST-LINK Utility.When I try to use the mode 'write protection', the application code works fine. When I try to use t...

STM32F7 internal SRAM Access

Posted on May 12, 2017 at 05:36Hello,I am using STM32F746IG. This has 320KB RAM - 64KB DTCM + 240KB(SRAM1) + 16KB(SRAM2)When my program uses 64KB, all the data is stored in DTCM and it all works fine. But when exceeds 64KB, data is stored in SRAM1(i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.