2017-05-08 7:55 AM
This package for this micro is a 36 pin WLCSP. The datasheet suggests on pg12 that it supports USB but not VDD_USB, unlike others in this range. Does this mean that the USB line voltage comes from normal VDD?
2017-05-12 8:28 AM
Hi Robert,
Indeed, for the devices were VDD_USB pin is not available, the USB transceiver and the two associated pads (PA11 and PA12) are powered by VDD;
You may refer to the relevant to your device (table 79) to have more information about the USB electrical characterstics thar you should respect.Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.